<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックHow to send 32-bit SPI using mpc5477 chip</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-send-32-bit-SPI-using-mpc5477-chip/m-p/1452711#M7251</link>
    <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I use Simulink to build the model. Its name is NXP_ MBDToolbox_ MPC57xx.&lt;/P&gt;&lt;P&gt;I want the master to send 32-bit data to the slave, but it only supports sending 16-bit data.&lt;/P&gt;&lt;P&gt;When I adjust the transfer size to 32, the oscilloscope displays abnormal.When I adjust the transfer size to 16, if I send 16 bits twice in a row, there will be a delay between SCKs.In the attachment are my model and the oscilloscope image when it is sent twice in a row.&lt;/P&gt;</description>
    <pubDate>Wed, 04 May 2022 12:29:57 GMT</pubDate>
    <dc:creator>CHAOWeiXu</dc:creator>
    <dc:date>2022-05-04T12:29:57Z</dc:date>
    <item>
      <title>How to send 32-bit SPI using mpc5477 chip</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-send-32-bit-SPI-using-mpc5477-chip/m-p/1452711#M7251</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I use Simulink to build the model. Its name is NXP_ MBDToolbox_ MPC57xx.&lt;/P&gt;&lt;P&gt;I want the master to send 32-bit data to the slave, but it only supports sending 16-bit data.&lt;/P&gt;&lt;P&gt;When I adjust the transfer size to 32, the oscilloscope displays abnormal.When I adjust the transfer size to 16, if I send 16 bits twice in a row, there will be a delay between SCKs.In the attachment are my model and the oscilloscope image when it is sent twice in a row.&lt;/P&gt;</description>
      <pubDate>Wed, 04 May 2022 12:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-send-32-bit-SPI-using-mpc5477-chip/m-p/1452711#M7251</guid>
      <dc:creator>CHAOWeiXu</dc:creator>
      <dc:date>2022-05-04T12:29:57Z</dc:date>
    </item>
  </channel>
</rss>