<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: I2C Slave Receive multiple bytes</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/I2C-Slave-Receive-multiple-bytes/m-p/1428474#M7095</link>
    <description>&lt;P&gt;I had to connect a data storage write with the same dimensions as number of bytes to receive. It is not possible to process the data directly.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="erde5544_0-1647344657140.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/173735iF55B62007EC8FCDD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="erde5544_0-1647344657140.png" alt="erde5544_0-1647344657140.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;erde5544_0-1647344657140.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Mar 2022 11:45:23 GMT</pubDate>
    <dc:creator>erde5544</dc:creator>
    <dc:date>2022-03-15T11:45:23Z</dc:date>
    <item>
      <title>I2C Slave Receive multiple bytes</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/I2C-Slave-Receive-multiple-bytes/m-p/1426871#M7089</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i'm using the MPC5748G Devkit and i want to communicate via I2C with a Raspberry Pi. The Devkit is the slave and i want to receive multiple bytes from the Master. But i only can receive the first byte, the other ones are lost. I tried with another Hardware as slave and it worked fine.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Am i doing something wrong in the configuration or is the hardware i2c timing not compatible?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I dont want to send the bytes seperately because of time loss.&lt;/P&gt;&lt;P&gt;Thanks for any help!&lt;/P&gt;</description>
      <pubDate>Fri, 11 Mar 2022 11:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/I2C-Slave-Receive-multiple-bytes/m-p/1426871#M7089</guid>
      <dc:creator>erde5544</dc:creator>
      <dc:date>2022-03-11T11:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave Receive multiple bytes</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/I2C-Slave-Receive-multiple-bytes/m-p/1428474#M7095</link>
      <description>&lt;P&gt;I had to connect a data storage write with the same dimensions as number of bytes to receive. It is not possible to process the data directly.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="erde5544_0-1647344657140.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/173735iF55B62007EC8FCDD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="erde5544_0-1647344657140.png" alt="erde5544_0-1647344657140.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;erde5544_0-1647344657140.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Mar 2022 11:45:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/I2C-Slave-Receive-multiple-bytes/m-p/1428474#M7095</guid>
      <dc:creator>erde5544</dc:creator>
      <dc:date>2022-03-15T11:45:23Z</dc:date>
    </item>
  </channel>
</rss>