<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mbd_s32k_get_config_param return is empty in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/mbd-s32k-get-config-param-return-is-empty/m-p/1424046#M7080</link>
    <description>&lt;P&gt;Making use of NXP_MBDToolbox_S32K1xx.&lt;/P&gt;&lt;P&gt;In lots of .tlc files the matlab function&amp;nbsp;mbd_s32k_get_config_param is used to retrieve the configuration parameters.&amp;nbsp; But the return is always empty and this results in errors in the code generation process.&lt;/P&gt;&lt;P&gt;As this is a .p function I can not see the content and can not judge on the cause of the error.&lt;/P&gt;&lt;P&gt;I tried both the config set in de model and a reference config set, but no success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See Diagnostic view information attached:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 08 Mar 2022 08:35:09 GMT</pubDate>
    <dc:creator>geertvenken</dc:creator>
    <dc:date>2022-03-08T08:35:09Z</dc:date>
    <item>
      <title>mbd_s32k_get_config_param return is empty</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/mbd-s32k-get-config-param-return-is-empty/m-p/1424046#M7080</link>
      <description>&lt;P&gt;Making use of NXP_MBDToolbox_S32K1xx.&lt;/P&gt;&lt;P&gt;In lots of .tlc files the matlab function&amp;nbsp;mbd_s32k_get_config_param is used to retrieve the configuration parameters.&amp;nbsp; But the return is always empty and this results in errors in the code generation process.&lt;/P&gt;&lt;P&gt;As this is a .p function I can not see the content and can not judge on the cause of the error.&lt;/P&gt;&lt;P&gt;I tried both the config set in de model and a reference config set, but no success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See Diagnostic view information attached:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Mar 2022 08:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/mbd-s32k-get-config-param-return-is-empty/m-p/1424046#M7080</guid>
      <dc:creator>geertvenken</dc:creator>
      <dc:date>2022-03-08T08:35:09Z</dc:date>
    </item>
  </channel>
</rss>