<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRun Time Error vs. Freemaster</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Run-Time-Error-vs-Freemaster/m-p/1421391#M7063</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is there a way to determine, whether an issue is a run time error due to the code or whether the issue is due to the connection to Freemaster or Freemaster settings?&lt;/P&gt;&lt;P&gt;My model after certain changes (extremely minor) will stop working after a certain period of time in Freemaster, but LED's continue to toggle and an oscilloscope shows that the board is still operating and timers are as expected.&lt;/P&gt;&lt;P&gt;An improvement was found by adjusting the Step Tick Priority and Polling Method for Freemaster, but the issues can still be generated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a method to debug with Freemaster?&amp;nbsp; Or is debugging in Freemaster, that the connection to the board is lost ([ERROR code=0x80000101]).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;</description>
    <pubDate>Tue, 01 Mar 2022 20:13:22 GMT</pubDate>
    <dc:creator>Sam_ECU</dc:creator>
    <dc:date>2022-03-01T20:13:22Z</dc:date>
    <item>
      <title>Run Time Error vs. Freemaster</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Run-Time-Error-vs-Freemaster/m-p/1421391#M7063</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is there a way to determine, whether an issue is a run time error due to the code or whether the issue is due to the connection to Freemaster or Freemaster settings?&lt;/P&gt;&lt;P&gt;My model after certain changes (extremely minor) will stop working after a certain period of time in Freemaster, but LED's continue to toggle and an oscilloscope shows that the board is still operating and timers are as expected.&lt;/P&gt;&lt;P&gt;An improvement was found by adjusting the Step Tick Priority and Polling Method for Freemaster, but the issues can still be generated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a method to debug with Freemaster?&amp;nbsp; Or is debugging in Freemaster, that the connection to the board is lost ([ERROR code=0x80000101]).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Mar 2022 20:13:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Run-Time-Error-vs-Freemaster/m-p/1421391#M7063</guid>
      <dc:creator>Sam_ECU</dc:creator>
      <dc:date>2022-03-01T20:13:22Z</dc:date>
    </item>
  </channel>
</rss>