<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic BMS &amp;amp; MBDT - RDDRONE-BMS772 MC33772B / S32K144 SPI COMMUNICATION FAULTS in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/BMS-amp-MBDT-RDDRONE-BMS772-MC33772B-S32K144-SPI-COMMUNICATION/m-p/1408558#M6953</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We try to communicate between MCU(S32K144 - 48Package) and MC33772B on board RDDRONE-BMS772 by using matlab simulink.&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all, we changed the oscillator on the board with an 8 MHz oscillator, since we couldn't select the Matlab Simulink "XTAL clock" value of 32 MHz.&lt;/P&gt;&lt;P&gt;Then we fed our board with a 6S battery pack (20.41Volt). &amp;nbsp;Since we wanted to measure 6 cells, we made the pin connections. Then, we set the mosfets, we got 20.41 volts from the output of the card.&lt;/P&gt;&lt;P&gt;We connected a 24 Volt 0.15A fan to the output of the card. There are differences between the values we get and the values we see in FreeMaster.&lt;/P&gt;&lt;P&gt;The cell voltage values we measured;&lt;BR /&gt;Cell_[0] : 3.391V&lt;BR /&gt;Cell_[1] : 3.405V&lt;BR /&gt;Cell_[2] : 3.406V&lt;BR /&gt;Cell_[3] : 3.407V&lt;BR /&gt;Cell_[4] : 3.406V&lt;BR /&gt;Cell_[5] : 3.399V&lt;/P&gt;&lt;P&gt;The Isense CURRENT value we measured; 120mA&lt;/P&gt;&lt;P&gt;Question 1) Why are the values of Cell Voltage lower than the real value in FreeMaster?? Especially ISENSE_CURRENT??&lt;/P&gt;&lt;P&gt;Question 2)&amp;nbsp;&lt;SPAN&gt;How do I fix these fault values? (HardwareFault values) ??&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Question 3)&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;When we send 0 value from Matlab simulink to the gate of the mosfet, we still measured 20.41 volts at the output. After some time (about 30 minutes), the output voltage dropped to 0.&lt;/SPAN&gt; &lt;SPAN class=""&gt;Why doesn't it drop to 0 instantly?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Oguz &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 03 Feb 2022 11:55:55 GMT</pubDate>
    <dc:creator>OGUZ1</dc:creator>
    <dc:date>2022-02-03T11:55:55Z</dc:date>
    <item>
      <title>BMS &amp; MBDT - RDDRONE-BMS772 MC33772B / S32K144 SPI COMMUNICATION FAULTS</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/BMS-amp-MBDT-RDDRONE-BMS772-MC33772B-S32K144-SPI-COMMUNICATION/m-p/1408558#M6953</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We try to communicate between MCU(S32K144 - 48Package) and MC33772B on board RDDRONE-BMS772 by using matlab simulink.&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all, we changed the oscillator on the board with an 8 MHz oscillator, since we couldn't select the Matlab Simulink "XTAL clock" value of 32 MHz.&lt;/P&gt;&lt;P&gt;Then we fed our board with a 6S battery pack (20.41Volt). &amp;nbsp;Since we wanted to measure 6 cells, we made the pin connections. Then, we set the mosfets, we got 20.41 volts from the output of the card.&lt;/P&gt;&lt;P&gt;We connected a 24 Volt 0.15A fan to the output of the card. There are differences between the values we get and the values we see in FreeMaster.&lt;/P&gt;&lt;P&gt;The cell voltage values we measured;&lt;BR /&gt;Cell_[0] : 3.391V&lt;BR /&gt;Cell_[1] : 3.405V&lt;BR /&gt;Cell_[2] : 3.406V&lt;BR /&gt;Cell_[3] : 3.407V&lt;BR /&gt;Cell_[4] : 3.406V&lt;BR /&gt;Cell_[5] : 3.399V&lt;/P&gt;&lt;P&gt;The Isense CURRENT value we measured; 120mA&lt;/P&gt;&lt;P&gt;Question 1) Why are the values of Cell Voltage lower than the real value in FreeMaster?? Especially ISENSE_CURRENT??&lt;/P&gt;&lt;P&gt;Question 2)&amp;nbsp;&lt;SPAN&gt;How do I fix these fault values? (HardwareFault values) ??&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Question 3)&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;When we send 0 value from Matlab simulink to the gate of the mosfet, we still measured 20.41 volts at the output. After some time (about 30 minutes), the output voltage dropped to 0.&lt;/SPAN&gt; &lt;SPAN class=""&gt;Why doesn't it drop to 0 instantly?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Oguz &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Feb 2022 11:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/BMS-amp-MBDT-RDDRONE-BMS772-MC33772B-S32K144-SPI-COMMUNICATION/m-p/1408558#M6953</guid>
      <dc:creator>OGUZ1</dc:creator>
      <dc:date>2022-02-03T11:55:55Z</dc:date>
    </item>
  </channel>
</rss>