<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: no CAN communication on MPC5744</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/no-CAN-communication-on-MPC5744/m-p/1386731#M6807</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193163"&gt;@hoeldMech&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I would first try to run a simple GPIO example to make sure that the code deployment, and the bord is working fine.&lt;/P&gt;
&lt;P&gt;Secondly, Can you tell me which are settings for the J43, J44 and J45 jumpers? I would try to put the J43, J44 and J45 on position 2-3 to set the external power for the MCU as well.&lt;/P&gt;
&lt;P&gt;Can you give both this a try?&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
    <pubDate>Tue, 14 Dec 2021 21:43:11 GMT</pubDate>
    <dc:creator>mariuslucianand</dc:creator>
    <dc:date>2021-12-14T21:43:11Z</dc:date>
    <item>
      <title>no CAN communication on MPC5744</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/no-CAN-communication-on-MPC5744/m-p/1384698#M6786</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I tried to send data from my simulink model over the onboard CAN pins (PB0, PB1) but I cannot get any valid information. Trying to read the signals with a Vector box I only get error frames.&lt;BR /&gt;So I tried to make the CAN example project "FlexCAN Master" running which does work neither. I use the MPC5744P RevE. Is it possible that any hardware changes between revB and revE make some issues?&lt;BR /&gt;An external power supply of 12 V is used.&lt;/P&gt;&lt;P&gt;Thank for your help!&lt;/P&gt;</description>
      <pubDate>Fri, 10 Dec 2021 08:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/no-CAN-communication-on-MPC5744/m-p/1384698#M6786</guid>
      <dc:creator>hoeldMech</dc:creator>
      <dc:date>2021-12-10T08:32:37Z</dc:date>
    </item>
    <item>
      <title>Re: no CAN communication on MPC5744</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/no-CAN-communication-on-MPC5744/m-p/1386731#M6807</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193163"&gt;@hoeldMech&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I would first try to run a simple GPIO example to make sure that the code deployment, and the bord is working fine.&lt;/P&gt;
&lt;P&gt;Secondly, Can you tell me which are settings for the J43, J44 and J45 jumpers? I would try to put the J43, J44 and J45 on position 2-3 to set the external power for the MCU as well.&lt;/P&gt;
&lt;P&gt;Can you give both this a try?&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 21:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/no-CAN-communication-on-MPC5744/m-p/1386731#M6807</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-12-14T21:43:11Z</dc:date>
    </item>
  </channel>
</rss>