<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 MCLIB for MPC564xL</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MCLIB-for-MPC564xL/m-p/1377567#M6751</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm having trouble using the GFLIB_Lut2D function from the MCLIB library for MPC564xL.&lt;/P&gt;&lt;P&gt;My intention is to generate code with the Simulink Embedded Coder. The problems I find are 3:&lt;/P&gt;&lt;P&gt;1) The parameters that must be passed to the function are 4, but in the documentation they only speak of 3. The parameter 's32MidId' does not appear in the documentation and I do not know what it means.&lt;/P&gt;&lt;P&gt;2) In the parameter 'ps32Table' if I write a matrix to it, it reports an error and tells me that it expects a vector.&lt;/P&gt;&lt;P&gt;3) In the generated code, the function parameters appear in code as hard code and my intention is that they are tunning parameters&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Fri, 26 Nov 2021 10:05:40 GMT</pubDate>
    <dc:creator>JavierGarrido</dc:creator>
    <dc:date>2021-11-26T10:05:40Z</dc:date>
    <item>
      <title>MCLIB for MPC564xL</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MCLIB-for-MPC564xL/m-p/1377567#M6751</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm having trouble using the GFLIB_Lut2D function from the MCLIB library for MPC564xL.&lt;/P&gt;&lt;P&gt;My intention is to generate code with the Simulink Embedded Coder. The problems I find are 3:&lt;/P&gt;&lt;P&gt;1) The parameters that must be passed to the function are 4, but in the documentation they only speak of 3. The parameter 's32MidId' does not appear in the documentation and I do not know what it means.&lt;/P&gt;&lt;P&gt;2) In the parameter 'ps32Table' if I write a matrix to it, it reports an error and tells me that it expects a vector.&lt;/P&gt;&lt;P&gt;3) In the generated code, the function parameters appear in code as hard code and my intention is that they are tunning parameters&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 26 Nov 2021 10:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MCLIB-for-MPC564xL/m-p/1377567#M6751</guid>
      <dc:creator>JavierGarrido</dc:creator>
      <dc:date>2021-11-26T10:05:40Z</dc:date>
    </item>
  </channel>
</rss>