<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: GPI Read input pin does not persist with save. Using MBDT for MPC57xx</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/GPI-Read-input-pin-does-not-persist-with-save-Using-MBDT-for/m-p/1356099#M6584</link>
    <description>&lt;P&gt;I found same issue with GPIO 456 and GPIO 196. MATLAB says it is the issue of&amp;nbsp; "MaskDisplay Command" , so it looks the issue of the MBDT library.&lt;/P&gt;</description>
    <pubDate>Fri, 15 Oct 2021 01:40:12 GMT</pubDate>
    <dc:creator>user_N</dc:creator>
    <dc:date>2021-10-15T01:40:12Z</dc:date>
    <item>
      <title>GPI Read input pin does not persist with save. Using MBDT for MPC57xx</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/GPI-Read-input-pin-does-not-persist-with-save-Using-MBDT-for/m-p/1220747#M5682</link>
      <description>&lt;P&gt;I am using NXP_MBDTToolbox_MPC57xx version 3.2.0 with R2020a. I am using the X-RDVCU5775EVM dev board which has the MPC5775B chip.&lt;/P&gt;&lt;P&gt;I have created a simple model to demonstrate the problem. All of the blocks are shown in the image below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Entire model.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135737i9C362DD9738BFFAC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Entire model.png" alt="Entire model.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; The input pin for the &lt;STRONG&gt;GPI Read&lt;/STRONG&gt; block is "PTG4: [SIU_A_GPIO196 | General Purpose I/O 196]" and is shown below.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Original settings.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135738iE0570D10BFB89F50/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Original settings.png" alt="Original settings.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; The model works as expected: when a board GPIO circuit is closed a board LED lights up. However, the problem occurs when I save the model and reopen it. When I reopen it the blocks look look like this. Question marks appear on the &lt;STRONG&gt;GPI Read&lt;/STRONG&gt; block mask. That is not the expected behavior.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Open after save.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135739iC6306A3B7C424D0A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Open after save.png" alt="Open after save.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; When I double-click on the GPI Read block the question marks are replaced by some text and an pin assignment is made that is not in agreement with the pin assignment I made before the file was saved.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="After double clicking GPI Read Block.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135740i6380EA96E01BDC2F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="After double clicking GPI Read Block.png" alt="After double clicking GPI Read Block.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; This is probably a bug. The behavior I expected was for the pin assignment I made before the file was saved to persist after I closed and then reopened the file.&lt;/P&gt;&lt;P&gt;I have attached my file. A fix would be appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 18:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/GPI-Read-input-pin-does-not-persist-with-save-Using-MBDT-for/m-p/1220747#M5682</guid>
      <dc:creator>ranulf</dc:creator>
      <dc:date>2021-01-25T18:04:17Z</dc:date>
    </item>
    <item>
      <title>Re: GPI Read input pin does not persist with save. Using MBDT for MPC57xx</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/GPI-Read-input-pin-does-not-persist-with-save-Using-MBDT-for/m-p/1226107#M5713</link>
      <description>&lt;P&gt;The ADP5589&amp;nbsp;is&amp;nbsp;a 19 I/O port expander with built-in&amp;nbsp;keypad Events&amp;nbsp;can&amp;nbsp;be&amp;nbsp;read&amp;nbsp;back by the processor via an I2C compatible interface. saving&amp;nbsp;board area and cost. Pin No. (LFCSP).&amp;nbsp;Pin No. (WLCSP) Mnemonic Description. 1. E3. R7. GPIO 8. This&amp;nbsp;pin&amp;nbsp;configure the general-purpose&amp;nbsp;input&amp;nbsp;(GPI) and logic activity.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 05:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/GPI-Read-input-pin-does-not-persist-with-save-Using-MBDT-for/m-p/1226107#M5713</guid>
      <dc:creator>Trevor145</dc:creator>
      <dc:date>2021-02-04T05:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: GPI Read input pin does not persist with save. Using MBDT for MPC57xx</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/GPI-Read-input-pin-does-not-persist-with-save-Using-MBDT-for/m-p/1356099#M6584</link>
      <description>&lt;P&gt;I found same issue with GPIO 456 and GPIO 196. MATLAB says it is the issue of&amp;nbsp; "MaskDisplay Command" , so it looks the issue of the MBDT library.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Oct 2021 01:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/GPI-Read-input-pin-does-not-persist-with-save-Using-MBDT-for/m-p/1356099#M6584</guid>
      <dc:creator>user_N</dc:creator>
      <dc:date>2021-10-15T01:40:12Z</dc:date>
    </item>
  </channel>
</rss>