<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to select Internal Clock in MBT for S32K116? in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-select-Internal-Clock-in-MBT-for-S32K116/m-p/1343965#M6522</link>
    <description>&lt;P&gt;I have Successfully downloaded and Installed the MBDtoolchain for Matlab Simulink, After selecting the MCU and opening the configuration for the MCU the parameter to select internal clock doesn't exist.&lt;BR /&gt;My requirement is to Select S32K116 MCU with Internal fast clock.&lt;BR /&gt;I have to integrate a BQ769x2 IC with this MCU, do we have a model desiged for this perticular IC? if not, how to add new Header file related to the Specific IC?&lt;/P&gt;</description>
    <pubDate>Wed, 22 Sep 2021 11:17:51 GMT</pubDate>
    <dc:creator>PrabhuNex</dc:creator>
    <dc:date>2021-09-22T11:17:51Z</dc:date>
    <item>
      <title>How to select Internal Clock in MBT for S32K116?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-select-Internal-Clock-in-MBT-for-S32K116/m-p/1343965#M6522</link>
      <description>&lt;P&gt;I have Successfully downloaded and Installed the MBDtoolchain for Matlab Simulink, After selecting the MCU and opening the configuration for the MCU the parameter to select internal clock doesn't exist.&lt;BR /&gt;My requirement is to Select S32K116 MCU with Internal fast clock.&lt;BR /&gt;I have to integrate a BQ769x2 IC with this MCU, do we have a model desiged for this perticular IC? if not, how to add new Header file related to the Specific IC?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 11:17:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-select-Internal-Clock-in-MBT-for-S32K116/m-p/1343965#M6522</guid>
      <dc:creator>PrabhuNex</dc:creator>
      <dc:date>2021-09-22T11:17:51Z</dc:date>
    </item>
    <item>
      <title>Re: How to select Internal Clock in MBT for S32K116?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-select-Internal-Clock-in-MBT-for-S32K116/m-p/1352113#M6561</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191598"&gt;@PrabhuNex&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;By default, the generated code for the S32K116 uses the external clock, settings made for the EVB board. If you want to change those settings, each time the code is generated, the&amp;nbsp;s32k_clock_init.c file is copied from the {Toolbox installation path}\mbdtbx_s32k11x\src\c_library. So you can change the settings in that file to use the&amp;nbsp;&lt;SPAN&gt;Internal fast clock. The C structure from the file is generated using the S32DS so you might find this information useful.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regarding the&amp;nbsp;BQ769x2 IC support, unfortunately, we do not provide support for that so if you want to include and use the custom code please have a look at this article&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-Battery-Management/ta-p/1119004" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-Battery-Management/ta-p/1119004&lt;/A&gt;&amp;nbsp;Also, in our toolbox you will find support for the MC3377xB Battery cell controller family so you might consider the usage of this MCU as well.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Thu, 07 Oct 2021 19:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-select-Internal-Clock-in-MBT-for-S32K116/m-p/1352113#M6561</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-10-07T19:33:47Z</dc:date>
    </item>
  </channel>
</rss>