<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: CAN/LIN not waking up after sleep</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1331965#M6444</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179775"&gt;@nidhin521&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Were you able to figure out a way to restore the communication without having to reset the board?&lt;/P&gt;</description>
    <pubDate>Mon, 30 Aug 2021 20:39:24 GMT</pubDate>
    <dc:creator>saranya_chitta</dc:creator>
    <dc:date>2021-08-30T20:39:24Z</dc:date>
    <item>
      <title>CAN/LIN not waking up after sleep</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1175510#M5231</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using Model based design toolset to implement CAN and LIN communication for a pump control software. I have an issue with CAN/LIN not waking up after it goes to sleep(Essentially I disconnect the CAN/LIN cables and plug it back in but the communication doesn't resume). Is there any way I can fix this issue?. Is there any way I can force wake up CAN/LIN using Model based design toolset&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Thu, 29 Oct 2020 21:32:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1175510#M5231</guid>
      <dc:creator>nidhin521</dc:creator>
      <dc:date>2020-10-29T21:32:27Z</dc:date>
    </item>
    <item>
      <title>Re: CAN/LIN not waking up after sleep</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1175755#M5234</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179775"&gt;@nidhin521&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;What low power mode are you using? IS the mcu refuses to wake up or the mcu wakes up but the communication is not working?&lt;/P&gt;
&lt;P&gt;Also, please have look at this thread. We have a great discussion here regarding the low power modes.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-put-S32K-MCU-into-sleep-low-power-mode/m-p/669711#M354" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-put-S32K-MCU-into-sleep-low-power-mode/m-p/669711#M354&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Oct 2020 08:08:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1175755#M5234</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2020-10-30T08:08:41Z</dc:date>
    </item>
    <item>
      <title>Re: CAN/LIN not waking up after sleep</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1175913#M5239</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for the quick response.&lt;/P&gt;&lt;P&gt;I haven't configured any power mode using MBDT. I am using S32K118 powered by external 12V. The board does both CAN and LIN communication. If I pull out the LIN cable, the CAN works fine, so I don't think the board is going into low power mode. Its just that the LIN doesnt work even on reconnecting the cable, until I reset the board. Same thing with CAN. if I pull out the CAN cable, LIN continues to work but CAN wont work even on reconnecting the cable until a board reset.&lt;/P&gt;&lt;P&gt;Is there any way I can reinitialize the CAN and LIN using MBDT or custom C code to restore the communication without resetting the board?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Oct 2020 16:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1175913#M5239</guid>
      <dc:creator>nidhin521</dc:creator>
      <dc:date>2020-10-30T16:53:59Z</dc:date>
    </item>
    <item>
      <title>Re: CAN/LIN not waking up after sleep</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1176033#M5241</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I went through the link you mentioned and figured out a way to reinitialize the LIN using LIN_DRV_Init(....)&amp;nbsp; function in System Outputs block. Working on reinitializing CAN the same way.&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Oct 2020 17:40:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1176033#M5241</guid>
      <dc:creator>nidhin521</dc:creator>
      <dc:date>2020-10-30T17:40:59Z</dc:date>
    </item>
    <item>
      <title>Re: CAN/LIN not waking up after sleep</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1331965#M6444</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179775"&gt;@nidhin521&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Were you able to figure out a way to restore the communication without having to reset the board?&lt;/P&gt;</description>
      <pubDate>Mon, 30 Aug 2021 20:39:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1331965#M6444</guid>
      <dc:creator>saranya_chitta</dc:creator>
      <dc:date>2021-08-30T20:39:24Z</dc:date>
    </item>
    <item>
      <title>Re: CAN/LIN not waking up after sleep</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1332317#M6448</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/132268"&gt;@saranya_chitta&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;As&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179775"&gt;@nidhin521&lt;/a&gt;&amp;nbsp;said, one way is to reinitialize the LIN, using custom code. But I think that trying to use the SDK function "LIN_DRV_AbortTransferData" would also work, using custom code.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Tue, 31 Aug 2021 07:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-LIN-not-waking-up-after-sleep/m-p/1332317#M6448</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-08-31T07:34:56Z</dc:date>
    </item>
  </channel>
</rss>