<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックMatlab generated code on S32DS ARM 2.2</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Matlab-generated-code-on-S32DS-ARM-2-2/m-p/1303810#M6282</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I get started to use NXP MBD tool for S32K142 with Matlab 2020b, I have created a simple model to test ADC and GPIO, I have build code on matlab downloading the code on the board without error. The problem is when I try to import the project on S32DS ARM 2.2 becouse I can't build code. Moreover I can't select the C/C++ Build window on project properties.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;Used tools:&lt;/P&gt;&lt;P&gt;NXP MDB toolbox 4.2.o&lt;/P&gt;&lt;P&gt;Matlab 2020b&lt;/P&gt;&lt;P&gt;S32DS ARM 2.2&lt;/P&gt;&lt;P&gt;Below I attach also the DS installation details.&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jul 2021 08:55:17 GMT</pubDate>
    <dc:creator>saiello</dc:creator>
    <dc:date>2021-07-07T08:55:17Z</dc:date>
    <item>
      <title>Matlab generated code on S32DS ARM 2.2</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Matlab-generated-code-on-S32DS-ARM-2-2/m-p/1303810#M6282</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I get started to use NXP MBD tool for S32K142 with Matlab 2020b, I have created a simple model to test ADC and GPIO, I have build code on matlab downloading the code on the board without error. The problem is when I try to import the project on S32DS ARM 2.2 becouse I can't build code. Moreover I can't select the C/C++ Build window on project properties.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;Used tools:&lt;/P&gt;&lt;P&gt;NXP MDB toolbox 4.2.o&lt;/P&gt;&lt;P&gt;Matlab 2020b&lt;/P&gt;&lt;P&gt;S32DS ARM 2.2&lt;/P&gt;&lt;P&gt;Below I attach also the DS installation details.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 08:55:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Matlab-generated-code-on-S32DS-ARM-2-2/m-p/1303810#M6282</guid>
      <dc:creator>saiello</dc:creator>
      <dc:date>2021-07-07T08:55:17Z</dc:date>
    </item>
  </channel>
</rss>