<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Restart PIL Simulation in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Restart-PIL-Simulation/m-p/1289928#M6134</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm facing the same issue. Or is there an option to bypass the flashing with the RAppID bootlader, e.g., by use S32 Design Studio to flash the board and "just" run the PiL simulation in Simulink?&lt;BR /&gt;Thanks for your answers.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jun 2021 13:23:35 GMT</pubDate>
    <dc:creator>patrick_schmid</dc:creator>
    <dc:date>2021-06-09T13:23:35Z</dc:date>
    <item>
      <title>Restart PIL Simulation</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Restart-PIL-Simulation/m-p/1286164#M6112</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm doing PIL simulations and everything works fine. However, downloading the application to the board using the RAppID bootloader everytime I rerun a simulation takes a long time.&lt;/P&gt;&lt;P&gt;Is there a way to simply restart the simulation in Simulink without needing to download the same model again to the board?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 14:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Restart-PIL-Simulation/m-p/1286164#M6112</guid>
      <dc:creator>hnkChinaski</dc:creator>
      <dc:date>2021-06-02T14:15:57Z</dc:date>
    </item>
    <item>
      <title>Re: Restart PIL Simulation</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Restart-PIL-Simulation/m-p/1289928#M6134</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm facing the same issue. Or is there an option to bypass the flashing with the RAppID bootlader, e.g., by use S32 Design Studio to flash the board and "just" run the PiL simulation in Simulink?&lt;BR /&gt;Thanks for your answers.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 13:23:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Restart-PIL-Simulation/m-p/1289928#M6134</guid>
      <dc:creator>patrick_schmid</dc:creator>
      <dc:date>2021-06-09T13:23:35Z</dc:date>
    </item>
    <item>
      <title>Re: Restart PIL Simulation</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Restart-PIL-Simulation/m-p/1291860#M6159</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I don't think the fast restart option helps with my problem. If I rerun a simulation with fast restart activated, the RAppID Bootlader will reflash the application first.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 10:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Restart-PIL-Simulation/m-p/1291860#M6159</guid>
      <dc:creator>hnkChinaski</dc:creator>
      <dc:date>2021-06-14T10:20:56Z</dc:date>
    </item>
  </channel>
</rss>