<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: SPI Setup Menu</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SPI-Setup-Menu/m-p/1282849#M6097</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Same thread is opened here&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/SPI-Setup-Menu/m-p/1282847#M6096" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/SPI-Setup-Menu/m-p/1282847#M6096&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Let's solve the issue there.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
    <pubDate>Wed, 26 May 2021 19:30:17 GMT</pubDate>
    <dc:creator>mariuslucianand</dc:creator>
    <dc:date>2021-05-26T19:30:17Z</dc:date>
    <item>
      <title>SPI Setup Menu</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SPI-Setup-Menu/m-p/1282391#M6089</link>
      <description>&lt;P&gt;What can we do to change these settings while running a program on the processor from the SPI setting menu shown in the picture?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ekran Alıntısı.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145549iA95D019983910657/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ekran Alıntısı.PNG" alt="Ekran Alıntısı.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ekran Alıntısı.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 08:13:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SPI-Setup-Menu/m-p/1282391#M6089</guid>
      <dc:creator>peaces</dc:creator>
      <dc:date>2021-05-26T08:13:59Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Setup Menu</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SPI-Setup-Menu/m-p/1282849#M6097</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Same thread is opened here&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/SPI-Setup-Menu/m-p/1282847#M6096" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/SPI-Setup-Menu/m-p/1282847#M6096&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Let's solve the issue there.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 19:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SPI-Setup-Menu/m-p/1282849#M6097</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-05-26T19:30:17Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Setup Menu</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SPI-Setup-Menu/m-p/1284080#M6108</link>
      <description>&lt;P&gt;They do this because this is the nature of SPI bus and this is how bus communications is done. Look:&lt;/P&gt;&lt;P&gt;Data transmission&lt;/P&gt;&lt;P&gt;Every SPI clock cycle is a full duplex data transmission. The master sends a bit on the MOSI pin and the slave reads it, while the slave sends a bit on the MISO pin and the master reads it. This sequence is true even if you only need an one-directional data transfer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.targetpayandbenefits.win/" target="_self"&gt;targetpayandbenefits&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 03:19:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SPI-Setup-Menu/m-p/1284080#M6108</guid>
      <dc:creator>Shawn442</dc:creator>
      <dc:date>2021-06-02T03:19:24Z</dc:date>
    </item>
  </channel>
</rss>