<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How can I use MBD for S32K to transmit/receive over 16 messages with different IDs in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-can-I-use-MBD-for-S32K-to-transmit-receive-over-16-messages/m-p/1280780#M6078</link>
    <description>&lt;P&gt;When I use&amp;nbsp;MBD for S32K to transmit/receive can messages. The number of messages are limited by the "can message buffer" as show in the figure below.&lt;/P&gt;&lt;P&gt;Or i will receive an error when building code.&lt;/P&gt;&lt;P&gt;"XXX is shared with another FlexCAN block with the same message box"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="bearman_m_0-1621823637819.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145290i0F8628027CF31513/image-size/medium?v=v2&amp;amp;px=400" role="button" title="bearman_m_0-1621823637819.png" alt="bearman_m_0-1621823637819.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so I can only send of receive 16 different messages,. When receiving , I can use mask, but when transmitting, there is no way i have found to change the IDset of the block.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;So is there any way i can transmit/receive over 16 can messages?&lt;/P&gt;&lt;P&gt;Thank you very much for your help.&lt;/P&gt;</description>
    <pubDate>Tue, 25 May 2021 00:59:01 GMT</pubDate>
    <dc:creator>bearman_m</dc:creator>
    <dc:date>2021-05-25T00:59:01Z</dc:date>
    <item>
      <title>How can I use MBD for S32K to transmit/receive over 16 messages with different IDs</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-can-I-use-MBD-for-S32K-to-transmit-receive-over-16-messages/m-p/1280780#M6078</link>
      <description>&lt;P&gt;When I use&amp;nbsp;MBD for S32K to transmit/receive can messages. The number of messages are limited by the "can message buffer" as show in the figure below.&lt;/P&gt;&lt;P&gt;Or i will receive an error when building code.&lt;/P&gt;&lt;P&gt;"XXX is shared with another FlexCAN block with the same message box"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="bearman_m_0-1621823637819.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/145290i0F8628027CF31513/image-size/medium?v=v2&amp;amp;px=400" role="button" title="bearman_m_0-1621823637819.png" alt="bearman_m_0-1621823637819.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so I can only send of receive 16 different messages,. When receiving , I can use mask, but when transmitting, there is no way i have found to change the IDset of the block.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;So is there any way i can transmit/receive over 16 can messages?&lt;/P&gt;&lt;P&gt;Thank you very much for your help.&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 00:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-can-I-use-MBD-for-S32K-to-transmit-receive-over-16-messages/m-p/1280780#M6078</guid>
      <dc:creator>bearman_m</dc:creator>
      <dc:date>2021-05-25T00:59:01Z</dc:date>
    </item>
    <item>
      <title>Re: How can I use MBD for S32K to transmit/receive over 16 messages with different IDs</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-can-I-use-MBD-for-S32K-to-transmit-receive-over-16-messages/m-p/1395190#M6848</link>
      <description>&lt;P&gt;Hi Bro&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Have you resolved your problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I'm also using mailbox to receive more than 16 can-fd msgs, maybe need a filter?&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 01:45:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-can-I-use-MBD-for-S32K-to-transmit-receive-over-16-messages/m-p/1395190#M6848</guid>
      <dc:creator>frank-li2021</dc:creator>
      <dc:date>2022-01-06T01:45:52Z</dc:date>
    </item>
    <item>
      <title>Re: How can I use MBD for S32K to transmit/receive over 16 messages with different IDs</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-can-I-use-MBD-for-S32K-to-transmit-receive-over-16-messages/m-p/1495618#M7546</link>
      <description>&lt;P&gt;hi bro:&lt;/P&gt;&lt;P&gt;thank you and it is true i can use filter to receive many messages with one receive block.&lt;/P&gt;&lt;P&gt;But i can not find the way to use one cansend block to send different messages with different IDs, in different time sequence.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 12:59:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-can-I-use-MBD-for-S32K-to-transmit-receive-over-16-messages/m-p/1495618#M7546</guid>
      <dc:creator>bearman_m</dc:creator>
      <dc:date>2022-07-26T12:59:21Z</dc:date>
    </item>
  </channel>
</rss>