<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Model reference: Make variables used but not defined in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-reference-Make-variables-used-but-not-defined/m-p/1271819#M6033</link>
    <description>&lt;P&gt;I see. Thank you for your help.&lt;/P&gt;</description>
    <pubDate>Tue, 04 May 2021 16:18:58 GMT</pubDate>
    <dc:creator>ruihang_wu</dc:creator>
    <dc:date>2021-05-04T16:18:58Z</dc:date>
    <item>
      <title>Model reference: Make variables used but not defined</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-reference-Make-variables-used-but-not-defined/m-p/1266815#M5999</link>
      <description>&lt;P&gt;I am trying to use model references in my project. If I compile the model without any references it works fine. But if I convert a subsystem to a model reference, error occur when compiling.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ruihang_wu_0-1619115083334.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/143008i7945A1923455D23F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ruihang_wu_0-1619115083334.png" alt="ruihang_wu_0-1619115083334.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ruihang_wu_0-1619115083334.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have double checked the system target file and the template makefile on the model reference are the same as the main project file. Is there anything I need to change when creating a model reference?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attached a simple test model where the error occurs during build&lt;/P&gt;</description>
      <pubDate>Thu, 22 Apr 2021 18:11:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-reference-Make-variables-used-but-not-defined/m-p/1266815#M5999</guid>
      <dc:creator>ruihang_wu</dc:creator>
      <dc:date>2021-04-22T18:11:46Z</dc:date>
    </item>
    <item>
      <title>Re: Model reference: Make variables used but not defined</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-reference-Make-variables-used-but-not-defined/m-p/1271735#M6032</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144167"&gt;@ruihang_wu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I am sorry for my delayed answer. Unfortunately, when it comes to reference models, the limitation we have on the S32K toolbox is that our main Configuration Block must also be in the reference models, even the referenced block has no NXP block in it. This should not affect the simulation.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Tue, 04 May 2021 14:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-reference-Make-variables-used-but-not-defined/m-p/1271735#M6032</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-05-04T14:02:43Z</dc:date>
    </item>
    <item>
      <title>Re: Model reference: Make variables used but not defined</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-reference-Make-variables-used-but-not-defined/m-p/1271819#M6033</link>
      <description>&lt;P&gt;I see. Thank you for your help.&lt;/P&gt;</description>
      <pubDate>Tue, 04 May 2021 16:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-reference-Make-variables-used-but-not-defined/m-p/1271819#M6033</guid>
      <dc:creator>ruihang_wu</dc:creator>
      <dc:date>2021-05-04T16:18:58Z</dc:date>
    </item>
  </channel>
</rss>