<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Measure PWM with MPC5777C? in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Measure-PWM-with-MPC5777C/m-p/1266748#M5997</link>
    <description>&lt;P&gt;The example provided enough information for me to develop code to measure PWM with the RDVCU5775EVM.&lt;/P&gt;</description>
    <pubDate>Thu, 22 Apr 2021 15:44:01 GMT</pubDate>
    <dc:creator>ranulf</dc:creator>
    <dc:date>2021-04-22T15:44:01Z</dc:date>
    <item>
      <title>Measure PWM with MPC5777C?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Measure-PWM-with-MPC5777C/m-p/1262143#M5982</link>
      <description>&lt;P&gt;I want to create and measure PWM signals with the RDVCU5775EVM, for which I use as the target, MPC5777C in the configuration block. Apparently, eMIOS is used to measure PWM signals for this target, but I don't see any examples demonstrating this. I would appreciate help finding relevant examples or a new example.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 16:31:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Measure-PWM-with-MPC5777C/m-p/1262143#M5982</guid>
      <dc:creator>ranulf</dc:creator>
      <dc:date>2021-04-14T16:31:06Z</dc:date>
    </item>
    <item>
      <title>Re: Measure PWM with MPC5777C?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Measure-PWM-with-MPC5777C/m-p/1262813#M5985</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179095"&gt;@ranulf&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;We should have an example in our toolbox which covers the input capture functionality. The model name is emios_ic_mpc5777c which uses the mpc5777c as target in the main config block.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please have a look at this model (also attached) and if this is not what you are looking for, we can discuss and I'll see what I can do.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 12:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Measure-PWM-with-MPC5777C/m-p/1262813#M5985</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-04-15T12:31:47Z</dc:date>
    </item>
    <item>
      <title>Re: Measure PWM with MPC5777C?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Measure-PWM-with-MPC5777C/m-p/1266748#M5997</link>
      <description>&lt;P&gt;The example provided enough information for me to develop code to measure PWM with the RDVCU5775EVM.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Apr 2021 15:44:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Measure-PWM-with-MPC5777C/m-p/1266748#M5997</guid>
      <dc:creator>ranulf</dc:creator>
      <dc:date>2021-04-22T15:44:01Z</dc:date>
    </item>
  </channel>
</rss>