<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K148 Soft Reset of CAN module in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K148-Soft-Reset-of-CAN-module/m-p/1248232#M5885</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;i am having the following issue:&lt;/P&gt;&lt;P&gt;While the CAN is active the physical connection is interrupted (TX and RX wiring). In that case i can see that fields &lt;STRONG&gt;ESR1(TXWRN) = 1b&lt;/STRONG&gt; and &lt;STRONG&gt;ESR1(FLTCONF) = 1b&lt;/STRONG&gt; are set. Reading that register is done by the "Read_Register" Block out of Simulink.&lt;/P&gt;&lt;P&gt;When TX and RX wires are connected aggain, the mentioned fields are still set and there are none CAN messages sendet by the controller.&lt;/P&gt;&lt;P&gt;I am trying to do an soft reset (set field &lt;STRONG&gt;MCR(SOFTRST) = 1b&lt;/STRONG&gt;) of the CAN controller to delete the mentioned fields. Writing that register is done by "Write_Register" Block out of Simulink.&lt;/P&gt;&lt;P&gt;But somehow setting of &lt;STRONG&gt;MCR(SOFTRST) = 1b&lt;/STRONG&gt; doesn't have any affect. The fields are still set and transmit of CAN messages is not working (receiving CAN messages seems to working).&lt;/P&gt;&lt;P&gt;Do anybody have an idea or any other solution to bring the CAN in normal mode aggain?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Denis&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 18 Mar 2021 14:09:26 GMT</pubDate>
    <dc:creator>DenisK</dc:creator>
    <dc:date>2021-03-18T14:09:26Z</dc:date>
    <item>
      <title>S32K148 Soft Reset of CAN module</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K148-Soft-Reset-of-CAN-module/m-p/1248232#M5885</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;i am having the following issue:&lt;/P&gt;&lt;P&gt;While the CAN is active the physical connection is interrupted (TX and RX wiring). In that case i can see that fields &lt;STRONG&gt;ESR1(TXWRN) = 1b&lt;/STRONG&gt; and &lt;STRONG&gt;ESR1(FLTCONF) = 1b&lt;/STRONG&gt; are set. Reading that register is done by the "Read_Register" Block out of Simulink.&lt;/P&gt;&lt;P&gt;When TX and RX wires are connected aggain, the mentioned fields are still set and there are none CAN messages sendet by the controller.&lt;/P&gt;&lt;P&gt;I am trying to do an soft reset (set field &lt;STRONG&gt;MCR(SOFTRST) = 1b&lt;/STRONG&gt;) of the CAN controller to delete the mentioned fields. Writing that register is done by "Write_Register" Block out of Simulink.&lt;/P&gt;&lt;P&gt;But somehow setting of &lt;STRONG&gt;MCR(SOFTRST) = 1b&lt;/STRONG&gt; doesn't have any affect. The fields are still set and transmit of CAN messages is not working (receiving CAN messages seems to working).&lt;/P&gt;&lt;P&gt;Do anybody have an idea or any other solution to bring the CAN in normal mode aggain?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Denis&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Mar 2021 14:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K148-Soft-Reset-of-CAN-module/m-p/1248232#M5885</guid>
      <dc:creator>DenisK</dc:creator>
      <dc:date>2021-03-18T14:09:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 Soft Reset of CAN module</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K148-Soft-Reset-of-CAN-module/m-p/1251001#M5893</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184663"&gt;@DenisK&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;The reported behavior looks to be similar to the one presented in this thread.&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Reset-CAN-Bus-Silence/m-p/1190321#M5426" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Reset-CAN-Bus-Silence/m-p/1190321#M5426&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Can you please give a try to this solution?&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 08:04:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K148-Soft-Reset-of-CAN-module/m-p/1251001#M5893</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-03-24T08:04:03Z</dc:date>
    </item>
  </channel>
</rss>