<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: MBDT import library error in MCSPTE1AK144</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-import-library-error-in-MCSPTE1AK144/m-p/1238668#M5838</link>
    <description>&lt;P&gt;thanks for the reply, I am trying to load and run V/F open loop method and in the Hardware setup it says to plug connector J9,J10 and J11 on position 2-3 ( will attach screenshot of the same below). My doubt is that V/F doesn't require any of the feedback then how the model works correctly?&lt;/P&gt;</description>
    <pubDate>Wed, 03 Mar 2021 05:17:08 GMT</pubDate>
    <dc:creator>RajG</dc:creator>
    <dc:date>2021-03-03T05:17:08Z</dc:date>
    <item>
      <title>MBDT import library error in MCSPTE1AK144</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-import-library-error-in-MCSPTE1AK144/m-p/1237523#M5805</link>
      <description>&lt;P&gt;&lt;FONT size="3"&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/50705"&gt;@Daniel_Popa&lt;/a&gt;&amp;nbsp; and all members, I am using MCSPTE1AK144 motor control toolkit. I have installed&amp;nbsp;&lt;STRONG&gt;MBDT v 4.2.0 with MATLAB R2018b, Simulink 9.2&lt;/STRONG&gt; but I am facing issues when I try to load the examples downloaded from&lt;EM&gt; Module 5 V/F Scalar Control&lt;/EM&gt; of "&amp;nbsp;&lt;/FONT&gt;&lt;FONT size="3"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;&lt;EM&gt;3-Phase PMSM Control Workshop with NXP's Model-Based Design Toolbox&lt;/EM&gt; "&lt;/SPAN&gt;. (I am downloading M5_2018.R1.zip file how ever I also tried with M5.zip and still show similar error)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;I will attach the screenshots so that it will be clear. I have also written my&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;query&amp;nbsp;&lt;/SPAN&gt;in image itself.&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT size="3"&gt;errors_simulink_0.png shows the warning when I open the file provided at bottom.&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT size="3"&gt;errors_simulink_1.png shows the two type of issues which I am facing.&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT size="3"&gt;errors_simulink_2.png shows that I can replace some type of block but cannot replace other types.&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;I have also posted this question of Module 5 page of workshop. Help me to understand the issues.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;RajG.&lt;/P&gt;</description>
      <pubDate>Sat, 27 Feb 2021 13:33:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-import-library-error-in-MCSPTE1AK144/m-p/1237523#M5805</guid>
      <dc:creator>RajG</dc:creator>
      <dc:date>2021-02-27T13:33:00Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT import library error in MCSPTE1AK144</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-import-library-error-in-MCSPTE1AK144/m-p/1237679#M5806</link>
      <description>&lt;P&gt;I suppose there was some issue when I uploaded the images, so here I am again re-uploading them.&lt;/P&gt;&lt;P&gt;Help me I am still stuck..&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;RajG.&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 04:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-import-library-error-in-MCSPTE1AK144/m-p/1237679#M5806</guid>
      <dc:creator>RajG</dc:creator>
      <dc:date>2021-03-01T04:44:34Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT import library error in MCSPTE1AK144</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-import-library-error-in-MCSPTE1AK144/m-p/1237877#M5813</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181122"&gt;@RajG&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;The models in the course are released in an older version of MBDT toolbox. The logic is the same but some blocks have to be manually replaced with the ones from the latest toolbox, like the new AMMCLIB blocks.&lt;/P&gt;
&lt;P&gt;You can find the final models already in the toolbox.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mariuslucianand_0-1614591476547.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138326i58FECDDFEFD4C0B4/image-size/large?v=v2&amp;amp;px=999" role="button" title="mariuslucianand_0-1614591476547.png" alt="mariuslucianand_0-1614591476547.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mariuslucianand_0-1614591476547.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 09:39:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-import-library-error-in-MCSPTE1AK144/m-p/1237877#M5813</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-03-01T09:39:08Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT import library error in MCSPTE1AK144</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-import-library-error-in-MCSPTE1AK144/m-p/1238668#M5838</link>
      <description>&lt;P&gt;thanks for the reply, I am trying to load and run V/F open loop method and in the Hardware setup it says to plug connector J9,J10 and J11 on position 2-3 ( will attach screenshot of the same below). My doubt is that V/F doesn't require any of the feedback then how the model works correctly?&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 05:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-import-library-error-in-MCSPTE1AK144/m-p/1238668#M5838</guid>
      <dc:creator>RajG</dc:creator>
      <dc:date>2021-03-03T05:17:08Z</dc:date>
    </item>
  </channel>
</rss>