<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC33771 OPEN-SHORT Detection in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-OPEN-SHORT-Detection/m-p/1231694#M5760</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/88067"&gt;@ykarata1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I had a look at the chapter you have mentioned above, which describes the steps which have to be followed to determine the Open-SHORT Detection, and unfortunately, the short answer is no. We do not have a block that performs all the mentioned steps in that chapter and return the OpenDetect status.&lt;/P&gt;
&lt;P&gt;However, the functionality can be achieved with the current toolbox in two ways:&lt;/P&gt;
&lt;P&gt;1. Using the&amp;nbsp;MC3377xB_Register_Read and&amp;nbsp;MC3377xB_Register_Write for&amp;nbsp;SYS_CFG1 and other registers. But you have to do all the operations inside an atomic subsystem and make sure that the Simulink will generate the code in the right order.&lt;/P&gt;
&lt;P&gt;2. Creating a custom code block that performs all the settings required in the mentioned chapter. Basically, here, the block has to be written in C and only called from the Simulink.&lt;/P&gt;
&lt;P&gt;If I were to choose, I would take the second option, with the custom code.&lt;/P&gt;
&lt;P&gt;For your second question, you can open a request at NXP to add support for such block.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 16 Feb 2021 18:45:54 GMT</pubDate>
    <dc:creator>mariuslucianand</dc:creator>
    <dc:date>2021-02-16T18:45:54Z</dc:date>
    <item>
      <title>MC33771 OPEN-SHORT Detection</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-OPEN-SHORT-Detection/m-p/1229911#M5745</link>
      <description>&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the datasheet of MC33771B, Part 9.9 , detection of short and open circuit in cell measurement cables has been told and described. Since we are proceeding as MBD on Simulink;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Do you have any block that we can use that detection ?&lt;/P&gt;&lt;P&gt;2. Are you able to support related block for S32K144 ?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 14:15:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-OPEN-SHORT-Detection/m-p/1229911#M5745</guid>
      <dc:creator>ykarata1</dc:creator>
      <dc:date>2021-02-11T14:15:13Z</dc:date>
    </item>
    <item>
      <title>Re: MC33771 OPEN-SHORT Detection</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-OPEN-SHORT-Detection/m-p/1231694#M5760</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/88067"&gt;@ykarata1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I had a look at the chapter you have mentioned above, which describes the steps which have to be followed to determine the Open-SHORT Detection, and unfortunately, the short answer is no. We do not have a block that performs all the mentioned steps in that chapter and return the OpenDetect status.&lt;/P&gt;
&lt;P&gt;However, the functionality can be achieved with the current toolbox in two ways:&lt;/P&gt;
&lt;P&gt;1. Using the&amp;nbsp;MC3377xB_Register_Read and&amp;nbsp;MC3377xB_Register_Write for&amp;nbsp;SYS_CFG1 and other registers. But you have to do all the operations inside an atomic subsystem and make sure that the Simulink will generate the code in the right order.&lt;/P&gt;
&lt;P&gt;2. Creating a custom code block that performs all the settings required in the mentioned chapter. Basically, here, the block has to be written in C and only called from the Simulink.&lt;/P&gt;
&lt;P&gt;If I were to choose, I would take the second option, with the custom code.&lt;/P&gt;
&lt;P&gt;For your second question, you can open a request at NXP to add support for such block.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Feb 2021 18:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-OPEN-SHORT-Detection/m-p/1231694#M5760</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-02-16T18:45:54Z</dc:date>
    </item>
    <item>
      <title>Re: MC33771 OPEN-SHORT Detection</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-OPEN-SHORT-Detection/m-p/1232830#M5765</link>
      <description>&lt;P&gt;Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply. Since we can not use Read/Write Register blocks only option we have seems as creating a custom code for on purpose. We will try to develop our own block. Since it will be first time for us, I believe it will take time.&lt;/P&gt;&lt;P&gt;Also I will open&amp;nbsp;&lt;SPAN&gt;a request at NXP to add support for such block.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 12:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771-OPEN-SHORT-Detection/m-p/1232830#M5765</guid>
      <dc:creator>ykarata1</dc:creator>
      <dc:date>2021-02-18T12:01:51Z</dc:date>
    </item>
  </channel>
</rss>