<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックMBDT Timed Subsystem</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-Timed-Subsystem/m-p/1225657#M5707</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have created a timed subsystem (1ms), within which sits two CAN Transmit blocks, a PWM Output block and an ADC Block, all joined together with a series of PI, P &amp;amp; I Controllers etc.&lt;/P&gt;&lt;P&gt;The CAN Tx blocks appear to behave as I'd expect them to do so; picking up and transmitting the relevant signals (as seen on CANalyzer)&lt;/P&gt;&lt;P&gt;The issue I'm having is with the CAN Rx block; almost regardless of what I do with it, the signal (see Simulink block diagram attached) doesn't reach the CAN Tx blocks, and is seen on CANalyzer as "0" when it should be within 20 and 80.&lt;/P&gt;&lt;P&gt;I've tried:&lt;/P&gt;&lt;P&gt;- Putting the CAN Rx area into a timed subsystem &amp;amp; using a rate transition block to connect the two subsystems&lt;/P&gt;&lt;P&gt;- Putting the CAN Rx area inside the timed subsystem&lt;/P&gt;&lt;P&gt;The only way this has worked for me thus far is when I don't have the timed subsystem at all. However, I need to have control over the CAN Tx times &amp;amp; control algorithm execution.&lt;/P&gt;&lt;P&gt;Any assistance is greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Crispin&lt;/P&gt;</description>
    <pubDate>Wed, 03 Feb 2021 15:20:43 GMT</pubDate>
    <dc:creator>C_Zuercher_APR</dc:creator>
    <dc:date>2021-02-03T15:20:43Z</dc:date>
    <item>
      <title>MBDT Timed Subsystem</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-Timed-Subsystem/m-p/1225657#M5707</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have created a timed subsystem (1ms), within which sits two CAN Transmit blocks, a PWM Output block and an ADC Block, all joined together with a series of PI, P &amp;amp; I Controllers etc.&lt;/P&gt;&lt;P&gt;The CAN Tx blocks appear to behave as I'd expect them to do so; picking up and transmitting the relevant signals (as seen on CANalyzer)&lt;/P&gt;&lt;P&gt;The issue I'm having is with the CAN Rx block; almost regardless of what I do with it, the signal (see Simulink block diagram attached) doesn't reach the CAN Tx blocks, and is seen on CANalyzer as "0" when it should be within 20 and 80.&lt;/P&gt;&lt;P&gt;I've tried:&lt;/P&gt;&lt;P&gt;- Putting the CAN Rx area into a timed subsystem &amp;amp; using a rate transition block to connect the two subsystems&lt;/P&gt;&lt;P&gt;- Putting the CAN Rx area inside the timed subsystem&lt;/P&gt;&lt;P&gt;The only way this has worked for me thus far is when I don't have the timed subsystem at all. However, I need to have control over the CAN Tx times &amp;amp; control algorithm execution.&lt;/P&gt;&lt;P&gt;Any assistance is greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Crispin&lt;/P&gt;</description>
      <pubDate>Wed, 03 Feb 2021 15:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-Timed-Subsystem/m-p/1225657#M5707</guid>
      <dc:creator>C_Zuercher_APR</dc:creator>
      <dc:date>2021-02-03T15:20:43Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT Timed Subsystem</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-Timed-Subsystem/m-p/1229294#M5739</link>
      <description>&lt;P&gt;Apologies; issue has been resolved. I hadn't included an initialisation area to take in the CAN Message and therefore trigger the function.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Feb 2021 12:36:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-Timed-Subsystem/m-p/1229294#M5739</guid>
      <dc:creator>C_Zuercher_APR</dc:creator>
      <dc:date>2021-02-10T12:36:39Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT Timed Subsystem</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-Timed-Subsystem/m-p/1229297#M5740</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182314"&gt;@C_Zuercher_APR&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Nice to hear this!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Wed, 10 Feb 2021 12:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-Timed-Subsystem/m-p/1229297#M5740</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-02-10T12:42:16Z</dc:date>
    </item>
  </channel>
</rss>