<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: CAN TIMEOUT DETECTION</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-TIMEOUT-DETECTION/m-p/1223265#M5697</link>
    <description>&lt;P&gt;TDR stands for&amp;nbsp;Timeout Detection&amp;nbsp;and Recovery. This is a feature of the Windows operating system which detects response problems from a graphics card, and recovers to a functional desktop by resetting the card.&lt;/P&gt;</description>
    <pubDate>Fri, 29 Jan 2021 12:07:20 GMT</pubDate>
    <dc:creator>WrightLyons</dc:creator>
    <dc:date>2021-01-29T12:07:20Z</dc:date>
    <item>
      <title>CAN TIMEOUT DETECTION</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-TIMEOUT-DETECTION/m-p/1173054#M5196</link>
      <description>&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;I need to detect whether I am getting heartbeat of other components that is connected through CAN communication. If not, I should give error after a timeout.&lt;/P&gt;&lt;P&gt;So while I am searching for a solution I have run into that thread. And I just wanted to implement recommended solution by&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/176411" target="_blank"&gt;@constantinrazva&lt;/A&gt;&amp;nbsp;in " &lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/CAN-Timing/m-p/1172473#M5178" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/CAN-Timing/m-p/1172473#M5178&lt;/A&gt; "&lt;/P&gt;&lt;P&gt;My block is here as it seems. I have put one Get_Bus_Tick in RX_Complete and One in Subsystem and substracted them to find timedifference. I am taking TIMEOUT as zero everytime.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also attached that part of my model like and excel file in attachment. You should convert attached file to .slx from xlsx.&lt;/P&gt;&lt;P&gt;How can I solve that?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 10:07:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-TIMEOUT-DETECTION/m-p/1173054#M5196</guid>
      <dc:creator>ykarata1</dc:creator>
      <dc:date>2020-10-26T10:07:48Z</dc:date>
    </item>
    <item>
      <title>Re: CAN TIMEOUT DETECTION</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-TIMEOUT-DETECTION/m-p/1173802#M5206</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I think I have an approximate solution for that. I am using timestamp output of RX block and checking has it changed or not by using change detection block. Also I am using Peridic Interrupt 1 and at each interrupt, it takes change detection as input. If three consecutive "not change" is detected, I raise a signal HIGH.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 11:17:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-TIMEOUT-DETECTION/m-p/1173802#M5206</guid>
      <dc:creator>ykarata1</dc:creator>
      <dc:date>2020-10-27T11:17:42Z</dc:date>
    </item>
    <item>
      <title>Re: CAN TIMEOUT DETECTION</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-TIMEOUT-DETECTION/m-p/1223265#M5697</link>
      <description>&lt;P&gt;TDR stands for&amp;nbsp;Timeout Detection&amp;nbsp;and Recovery. This is a feature of the Windows operating system which detects response problems from a graphics card, and recovers to a functional desktop by resetting the card.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jan 2021 12:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-TIMEOUT-DETECTION/m-p/1223265#M5697</guid>
      <dc:creator>WrightLyons</dc:creator>
      <dc:date>2021-01-29T12:07:20Z</dc:date>
    </item>
  </channel>
</rss>