<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 Bit Rate Switch functionality</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Bit-Rate-Switch-functionality/m-p/1220528#M5681</link>
    <description>&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;I am working with a s32k146 board on the implementation of a CAN FD system. When I send and receive CAN FD messages it works just fine.&lt;/P&gt;&lt;P&gt;The problem is when I try to use the BRS on these CAN FD messages. If I use a model in which I try to send/receive CAN FD messages to/from my CAN Tool with the BRS, it doesn't work. If I use the exact same model without the BRS active it works just fine.&lt;/P&gt;&lt;P&gt;I tried modifying the .tlc and mask of the block and linkinf them to the correspondant functions but it didn't work so I guess something more complicated is happening.&lt;/P&gt;&lt;P&gt;Can I get a hint on what could be happening? Is this a pending functionality?&lt;/P&gt;&lt;P&gt;Thanks MBD team.&lt;/P&gt;</description>
    <pubDate>Mon, 25 Jan 2021 12:24:38 GMT</pubDate>
    <dc:creator>juliana_rojas30</dc:creator>
    <dc:date>2021-01-25T12:24:38Z</dc:date>
    <item>
      <title>Bit Rate Switch functionality</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Bit-Rate-Switch-functionality/m-p/1220528#M5681</link>
      <description>&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;I am working with a s32k146 board on the implementation of a CAN FD system. When I send and receive CAN FD messages it works just fine.&lt;/P&gt;&lt;P&gt;The problem is when I try to use the BRS on these CAN FD messages. If I use a model in which I try to send/receive CAN FD messages to/from my CAN Tool with the BRS, it doesn't work. If I use the exact same model without the BRS active it works just fine.&lt;/P&gt;&lt;P&gt;I tried modifying the .tlc and mask of the block and linkinf them to the correspondant functions but it didn't work so I guess something more complicated is happening.&lt;/P&gt;&lt;P&gt;Can I get a hint on what could be happening? Is this a pending functionality?&lt;/P&gt;&lt;P&gt;Thanks MBD team.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 12:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Bit-Rate-Switch-functionality/m-p/1220528#M5681</guid>
      <dc:creator>juliana_rojas30</dc:creator>
      <dc:date>2021-01-25T12:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: Bit Rate Switch functionality</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Bit-Rate-Switch-functionality/m-p/1228176#M5734</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/148298"&gt;@juliana_rojas30&lt;/a&gt; ,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Indeed, the CAN FD with BRS isn't working. It seems that all register fields used for CAN bitrate are incremented by 1 when used by the hardware, except one, FDCBT[FPROPSEG]. So we don't need to subtract 1 from the value set in the FCAN_Config.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I attached a cumulative patch, a self-extracting archive, that contains the fix for this issue and the previous patch from &lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/CAN-FD-in-S32k14x-EVB/m-p/1212388" target="_self"&gt;CAN FD in S32k14x EVB&lt;/A&gt; .&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The steps to apply the patch:&lt;/P&gt;
&lt;P&gt;1. Download the attached zip file and unzip it.&lt;/P&gt;
&lt;P&gt;2. Run &lt;STRONG&gt;mbd_find_s32k_root&lt;/STRONG&gt;() to get the root folder there the S32K toolbox is installed.&lt;/P&gt;
&lt;P&gt;3. Close Matlab.&lt;/P&gt;
&lt;P&gt;4. Open the &lt;STRONG&gt;&lt;SPAN class="lia-link-navigation lia-attachment-link lia-link-disabled"&gt;MBDToolbox_S32K1xx_4.2.0_can_fd_patch_2.&lt;/SPAN&gt;exe&lt;/STRONG&gt; file and extract it's contents to the root folder of the toolbox.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Paul&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 18:03:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Bit-Rate-Switch-functionality/m-p/1228176#M5734</guid>
      <dc:creator>paulvlase</dc:creator>
      <dc:date>2021-02-08T18:03:40Z</dc:date>
    </item>
  </channel>
</rss>