<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issue to read pack current using (FRDM33771BTPL and FRDM33664BEVB) with a single TPL Device in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-to-read-pack-current-using-FRDM33771BTPL-and-FRDM33664BEVB/m-p/1199879#M5493</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180634"&gt;@NPXLONG&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I am glad that your issue is now solved!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
    <pubDate>Tue, 15 Dec 2020 20:07:47 GMT</pubDate>
    <dc:creator>mariuslucianand</dc:creator>
    <dc:date>2020-12-15T20:07:47Z</dc:date>
    <item>
      <title>Issue to read pack current using (FRDM33771BTPL and FRDM33664BEVB) with a single TPL Device</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-to-read-pack-current-using-FRDM33771BTPL-and-FRDM33664BEVB/m-p/1199448#M5489</link>
      <description>&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I received the BMS development kits for (SPI 6-cells and TPL 14-cells) options. Meanwhile I am still waiting for the second device of TPL chain. I tried the SPI 6-cells BMS and the measure output results are working as expected. I can read "packvoltage, packcurrent, 6-cells voltage and NTC temperature.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In addition, I tested the TPL 14-cells with a single device and able to measure up to 14-cells voltage value, total Packvoltage and NTC temperature too. Apart from that, I have some issue to read the pack current &lt;FONT color="#0000FF"&gt;(See attached - Single_TPL..., BMS_Single...., Single_MC33771TPL.slx and .pmpx)&lt;/FONT&gt;. The packcurrent on freemaster always displayed at "0". I was wondering whether my 33771BTPL or 14emulator hardware failure? or my Simulink wrong settings?&amp;nbsp; I checked the resistance for each of the hardware slider using a multimeter. Since, I was able to read all the 14 cells voltage except the pack current.&amp;nbsp;@&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088" target="_self"&gt;mariuslucianand&lt;/A&gt;, I hoping that on your side can try to run the device test for my Simulink R2018B file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;However, 6 cells SPI setup has no issue to read all the parameters. &lt;FONT color="#0000FF"&gt;(See-attached: Single SPI.....)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I read the following tutorials to ensure that I can properly configured all the hardware wire connection:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/BMS-amp-MBDT-MC33771B-MC33772B-SPI-communication-with-S32K/ta-p/1152835" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/BMS-amp-MBDT-MC33771B-MC33772B-SPI-communication-with-S32K/ta-p/1152835&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/BMS-amp-MBDT-MC33771B-MC33772B-TPL-communication-with-S32K/ta-p/1153459" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/BMS-amp-MBDT-MC33771B-MC33772B-TPL-communication-with-S32K/ta-p/1153459&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and the&amp;nbsp;&lt;SPAN&gt;UM1143&amp;nbsp;for the&amp;nbsp;33664 jumper wire connections.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks for your helping&amp;nbsp;&lt;SPAN class=""&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;. I look forward to hearing from your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 07:42:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-to-read-pack-current-using-FRDM33771BTPL-and-FRDM33664BEVB/m-p/1199448#M5489</guid>
      <dc:creator>NPXLONG</dc:creator>
      <dc:date>2020-12-15T07:42:37Z</dc:date>
    </item>
    <item>
      <title>Re: Issue to read pack current using (FRDM33771BTPL and FRDM33664BEVB) with a single TPL Device</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-to-read-pack-current-using-FRDM33771BTPL-and-FRDM33664BEVB/m-p/1199568#M5490</link>
      <description>&lt;P&gt;Hi Marius,&lt;/P&gt;&lt;P&gt;I made the simple mistake to set the second device instead of one device on the&amp;nbsp;MC3377xB_Config. So my problem is solved.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 09:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-to-read-pack-current-using-FRDM33771BTPL-and-FRDM33664BEVB/m-p/1199568#M5490</guid>
      <dc:creator>NPXLONG</dc:creator>
      <dc:date>2020-12-15T09:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: Issue to read pack current using (FRDM33771BTPL and FRDM33664BEVB) with a single TPL Device</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-to-read-pack-current-using-FRDM33771BTPL-and-FRDM33664BEVB/m-p/1199879#M5493</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180634"&gt;@NPXLONG&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I am glad that your issue is now solved!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 20:07:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-to-read-pack-current-using-FRDM33771BTPL-and-FRDM33664BEVB/m-p/1199879#M5493</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2020-12-15T20:07:47Z</dc:date>
    </item>
  </channel>
</rss>