<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 Re: Flash EEE Read and Write</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1178059#M5267</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144167"&gt;@ruihang_wu&lt;/a&gt; , &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12402"&gt;@Maciek&lt;/a&gt; , &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/147016"&gt;@oeren5&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The problem is that we didn't multiple the size of the input data buffer by the size of the selected data type.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you try the following fix:&lt;/P&gt;
&lt;P&gt;1. Unzip the attached &lt;STRONG&gt;&lt;SPAN class="lia-link-navigation lia-attachment-link lia-link-disabled"&gt;flash_s32k_eeewrite.zip &lt;/SPAN&gt;&lt;/STRONG&gt;file.&lt;/P&gt;
&lt;P&gt;1. Copy &lt;SPAN class="lia-link-navigation lia-attachment-link lia-link-disabled"&gt;flash_s32k_eeewrite.tlc &lt;/SPAN&gt;file to &amp;lt;&lt;STRONG&gt;TBX_ROOT&amp;gt;\&lt;/STRONG&gt;&lt;STRONG&gt;src\mbdtbx_s32k\blocks\flash&lt;/STRONG&gt; folder, where &lt;STRONG&gt;&amp;lt;TBX_ROOT&amp;gt; &lt;/STRONG&gt;is the output of &lt;STRONG&gt;mbd_find_s32k_root().&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;2. Build and run your model.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Paul&lt;/P&gt;</description>
    <pubDate>Wed, 04 Nov 2020 16:44:42 GMT</pubDate>
    <dc:creator>paulvlase</dc:creator>
    <dc:date>2020-11-04T16:44:42Z</dc:date>
    <item>
      <title>Flash EEE Read and Write</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1170584#M5164</link>
      <description>&lt;P&gt;I'm using the EEERead and EEEWrite block to store data to nonvolatile memory. Reading from the address is not a problem. However I'm seeing only the last 8 bit being written. I have 3 uint16 variables, They are stored using the flash EEEWrite block with offset 0x0000, 0x0002, 0x0004. Using FreeMaster I only see the last 8 bit of 0x14000000, 0x14000002, and 0x14000004 change, but the first 8 bit always remains 11111111, effectively losing the first 8 bits when I am reading from those addresses again.&lt;/P&gt;&lt;P&gt;I have tried setting the type to uint32 but it's still only the last 8 bits that gets saved.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attached the freemaster and simulink files as reference.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 01:02:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1170584#M5164</guid>
      <dc:creator>ruihang_wu</dc:creator>
      <dc:date>2020-10-21T01:02:52Z</dc:date>
    </item>
    <item>
      <title>Re: Flash EEE Read and Write</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1171888#M5173</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;This is Ozan and I experienced similar problem with Flash EEE read and write blocks. S32K144EVB, mbdt v4.2 and Simulink 2020a is used.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I try to store 14 different data in non-volatile memory and then read the data and I could not succeed it. Normally I will use a vector with 14 elements and I use a selector to select the indented element. But for now I used 14 constant in order to test the ability. I basically write 14 constants (in type uint32) to non volatile memory with offset values 0x000, 0x0010, 0x0020...... 0x0130. Then I used Flash EEERead block to read this values and write them in to volatile memory. I used Freemaster to read the values from both volatile memory blocks (write_valx) and non-volatile address but both show different values than the ones that I used.&amp;nbsp;&lt;STRONG&gt;How can I solve this problem and store multiple different data?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The screenshots of model are provided below.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oeren5_0-1603374248832.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128047i12478818976F437F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="oeren5_0-1603374248832.png" alt="oeren5_0-1603374248832.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oeren5_1-1603374275718.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128048iAEC5B49EFE88BD71/image-size/medium?v=v2&amp;amp;px=400" role="button" title="oeren5_1-1603374275718.png" alt="oeren5_1-1603374275718.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oeren5_2-1603374302337.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128049iC9AF00B2D6D2B995/image-size/medium?v=v2&amp;amp;px=400" role="button" title="oeren5_2-1603374302337.png" alt="oeren5_2-1603374302337.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oeren5_3-1603375327325.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128051i96657DCA47DB082B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="oeren5_3-1603375327325.png" alt="oeren5_3-1603375327325.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oeren5_4-1603375345369.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128052i92772B68A92A842D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="oeren5_4-1603375345369.png" alt="oeren5_4-1603375345369.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Oct 2020 14:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1171888#M5173</guid>
      <dc:creator>oeren5</dc:creator>
      <dc:date>2020-10-22T14:04:27Z</dc:date>
    </item>
    <item>
      <title>Re: Flash EEE Read and Write</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1172501#M5179</link>
      <description>&lt;P&gt;I can confirm similar behavior. Using Memory monitor in S32K Design Studio, on custom board with S32K116, we have seen that writing uint32 value results in writing correctly only the lowest significant byte.&lt;/P&gt;&lt;P&gt;But reading and writing uint8 values works fine.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Oct 2020 14:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1172501#M5179</guid>
      <dc:creator>Maciek</dc:creator>
      <dc:date>2020-10-23T14:06:56Z</dc:date>
    </item>
    <item>
      <title>Re: Flash EEE Read and Write</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1172942#M5190</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24319"&gt;@paulvlase&lt;/a&gt;&amp;nbsp;, Can you comment on this?&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 07:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1172942#M5190</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2020-10-26T07:59:13Z</dc:date>
    </item>
    <item>
      <title>Re: Flash EEE Read and Write</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1174551#M5218</link>
      <description>&lt;P&gt;I worked around the problem for now by slicing the variable to uint8 and saving that. And concatenating the two halves when reading.&lt;/P&gt;&lt;P&gt;The variable was changed to int16 for unrelated reasons.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2020-10-28 092940.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128528i701667E4982D4AD3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot 2020-10-28 092940.png" alt="Screenshot 2020-10-28 092940.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2020-10-28 093342.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128529iCC3F857CD8F147E6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot 2020-10-28 093342.png" alt="Screenshot 2020-10-28 093342.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Another work around would be to follow this example&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-Battery-Management/ta-p/1119004" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-Battery-Management/ta-p/1119004&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and apply the C code from this example&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/EXAMPLE-S32K144-EEEPROM-usage-No-SDK/ta-p/1106848" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/EXAMPLE-S32K144-EEEPROM-usage-No-SDK/ta-p/1106848&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The matlab S function blocks will handle the read and write in this case.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I guess these are the two ways to go about it until the block is updated.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 13:46:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1174551#M5218</guid>
      <dc:creator>ruihang_wu</dc:creator>
      <dc:date>2020-10-28T13:46:34Z</dc:date>
    </item>
    <item>
      <title>Re: Flash EEE Read and Write</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1178059#M5267</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144167"&gt;@ruihang_wu&lt;/a&gt; , &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12402"&gt;@Maciek&lt;/a&gt; , &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/147016"&gt;@oeren5&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The problem is that we didn't multiple the size of the input data buffer by the size of the selected data type.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you try the following fix:&lt;/P&gt;
&lt;P&gt;1. Unzip the attached &lt;STRONG&gt;&lt;SPAN class="lia-link-navigation lia-attachment-link lia-link-disabled"&gt;flash_s32k_eeewrite.zip &lt;/SPAN&gt;&lt;/STRONG&gt;file.&lt;/P&gt;
&lt;P&gt;1. Copy &lt;SPAN class="lia-link-navigation lia-attachment-link lia-link-disabled"&gt;flash_s32k_eeewrite.tlc &lt;/SPAN&gt;file to &amp;lt;&lt;STRONG&gt;TBX_ROOT&amp;gt;\&lt;/STRONG&gt;&lt;STRONG&gt;src\mbdtbx_s32k\blocks\flash&lt;/STRONG&gt; folder, where &lt;STRONG&gt;&amp;lt;TBX_ROOT&amp;gt; &lt;/STRONG&gt;is the output of &lt;STRONG&gt;mbd_find_s32k_root().&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;2. Build and run your model.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Paul&lt;/P&gt;</description>
      <pubDate>Wed, 04 Nov 2020 16:44:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1178059#M5267</guid>
      <dc:creator>paulvlase</dc:creator>
      <dc:date>2020-11-04T16:44:42Z</dc:date>
    </item>
    <item>
      <title>Re: Flash EEE Read and Write</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1178254#M5270</link>
      <description>&lt;P&gt;It works with all the data types I tested if I create a new model. But if I change change one of the existing models I get an unspecified error.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ruihang_wu_1-1604524037782.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/129118iBFE22C289DB4D632/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ruihang_wu_1-1604524037782.png" alt="ruihang_wu_1-1604524037782.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I tried deleting the generated mbd_rtw folder and I get the same message.&lt;/P&gt;&lt;P&gt;Wondering if &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12402"&gt;@Maciek&lt;/a&gt; and &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/147016"&gt;@oeren5&lt;/a&gt; are seeing the same thing&lt;/P&gt;</description>
      <pubDate>Wed, 04 Nov 2020 21:11:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1178254#M5270</guid>
      <dc:creator>ruihang_wu</dc:creator>
      <dc:date>2020-11-04T21:11:11Z</dc:date>
    </item>
  </channel>
</rss>