<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What CAN channels are Supported by Simulink on the dev board X-RDVCU5775EVM Ver B? in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/What-CAN-channels-are-Supported-by-Simulink-on-the-dev-board-X/m-p/1173377#M5200</link>
    <description>&lt;P&gt;I am using:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Windows 10&lt;/LI&gt;&lt;LI&gt;MATLAB/Simulink 2020a&lt;/LI&gt;&lt;LI&gt;MBDT version 3.2.0&lt;/LI&gt;&lt;LI&gt;The dev board X-RDVCU5775EVM Ver B, which has the MPC5775B chip&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;With the target set at MPC5777C in the 'MBD_MPC574x_Config_Information' block I have only been able to get one of the CAN channels to work:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;In Simulink: 'FCAN Module: 0'&lt;/LI&gt;&lt;LI&gt;On the 130-pin ECU Cable: (CAN1_L, C12) and (CAN1_H, D12)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I would expect the channel at [(CAN2_L, C13) and (CAN2_H, D13)] and the channel at [(SBC_CAN_L, C11) and (SBC_CAN_H, D11)] to also work. So far, I have not been able to make these other channels work.&lt;/P&gt;&lt;P&gt;Are these other CAN channels on the dev board known to work with Simulink?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 26 Oct 2020 22:17:14 GMT</pubDate>
    <dc:creator>ranulf</dc:creator>
    <dc:date>2020-10-26T22:17:14Z</dc:date>
    <item>
      <title>What CAN channels are Supported by Simulink on the dev board X-RDVCU5775EVM Ver B?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/What-CAN-channels-are-Supported-by-Simulink-on-the-dev-board-X/m-p/1173377#M5200</link>
      <description>&lt;P&gt;I am using:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Windows 10&lt;/LI&gt;&lt;LI&gt;MATLAB/Simulink 2020a&lt;/LI&gt;&lt;LI&gt;MBDT version 3.2.0&lt;/LI&gt;&lt;LI&gt;The dev board X-RDVCU5775EVM Ver B, which has the MPC5775B chip&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;With the target set at MPC5777C in the 'MBD_MPC574x_Config_Information' block I have only been able to get one of the CAN channels to work:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;In Simulink: 'FCAN Module: 0'&lt;/LI&gt;&lt;LI&gt;On the 130-pin ECU Cable: (CAN1_L, C12) and (CAN1_H, D12)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I would expect the channel at [(CAN2_L, C13) and (CAN2_H, D13)] and the channel at [(SBC_CAN_L, C11) and (SBC_CAN_H, D11)] to also work. So far, I have not been able to make these other channels work.&lt;/P&gt;&lt;P&gt;Are these other CAN channels on the dev board known to work with Simulink?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 22:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/What-CAN-channels-are-Supported-by-Simulink-on-the-dev-board-X/m-p/1173377#M5200</guid>
      <dc:creator>ranulf</dc:creator>
      <dc:date>2020-10-26T22:17:14Z</dc:date>
    </item>
  </channel>
</rss>