<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k144 EVB CAN Communication using MBD in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1164583#M5118</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;This solution worked for me with one controller. But something went wrong with the controller and I was not able to fix it. So I purchased a new controller, now I am not able to verify CAN communication. I used Vector CANAlyzer but I do not see any communication. I have 12V connected to the board and Pin J107 (1-2) are also connected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please help me what else I can do?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the problem I had with my old controller and was not able to fix: &lt;FONT&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K144-not-working/m-p/1160684" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K/S32K144-not-working/m-p/1160684&lt;/A&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Oct 2020 14:44:11 GMT</pubDate>
    <dc:creator>parveez</dc:creator>
    <dc:date>2020-10-08T14:44:11Z</dc:date>
    <item>
      <title>S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057694#M4497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to send CAN message with 4 signals. These signals should be sent in Motorola format and I want to pack the data in the following format.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following shows the layout for CAN message:&lt;/P&gt;&lt;P&gt;&lt;IMG height="146" width="266" /&gt;&lt;/P&gt;&lt;P&gt;Can you please let me know how can I achieve this with the NXP MBD toolbox in MATLAB?&lt;/P&gt;&lt;P&gt;Is there a way I can use the dbc file directly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rubeena&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Aug 2020 23:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057694#M4497</guid>
      <dc:creator>rparveez</dc:creator>
      <dc:date>2020-08-23T23:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057695#M4498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rparveez@mtu.edu"&gt;rparveez@mtu.edu&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately you can't use a dbc file for now -- we're looking into expanding the support to cover that as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sorry but I can't see the image you posted. With our toolbox, you can just input the data you want to send, the ID you want it to have and set-up if you want standard or extended format and if you need it to have RTR set. From this information, the whole CAN frame is put together and sent over the CAN bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a video that goes through some examples, after a brief introduction of the CAN protocol -- might find some answers there. You can find it &lt;A href="https://www.nxp.com/design/training/introducing-the-can-communication-blocks-from-nxp-mbdt:TIP-INTRODUCING-THE-CAN-COMMUNICATION-BLOCKS"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2020 07:54:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057695#M4498</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2020-08-24T07:54:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057696#M4499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/constantinrazvan.chivu"&gt;constantinrazvan.chivu&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have another question, can I have S32K144 EVB CAN communicate with other devices and view CAN and other parameters/calibrations on FreeMaster?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rubeena&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2020 17:44:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057696#M4499</guid>
      <dc:creator>rparveez</dc:creator>
      <dc:date>2020-08-24T17:44:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057697#M4500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rparveez@mtu.edu"&gt;rparveez@mtu.edu&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you can certainly have S32K144 EVB communicate on any CAN bus with other devices - you just have to make the physical connections. Regarding the 2nd part of the question, yes, you can view and modify parameters using FreeMASTER - the only thing you should do is add the FreeMASTER Config block into your model. You can start from one of our examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2020 08:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057697#M4500</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2020-08-25T08:09:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057698#M4501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;‌&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/constantinrazvan.chivu"&gt;constantinrazvan.chivu&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;I tried this, the FreeMaster config to use LPUART0 and FCAN module:0&lt;/P&gt;&lt;P&gt;After building and downloading the code, the FreeMaster does not connect to the board.&lt;/P&gt;&lt;P&gt;Also, I have blue LED to blink once code is downloaded. This doesn't work either.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try building other modules which did not have CAN communication blocks, the FreeMaster connected to the board and the blue LED blinks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure what is the problem, is it due to CAN config? Do you have an examples where two devices communicate over CAN and some parameters that on FreeMaster?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rubeena&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2020 19:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057698#M4501</guid>
      <dc:creator>rparveez</dc:creator>
      <dc:date>2020-08-25T19:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057699#M4502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rparveez@mtu.edu"&gt;rparveez@mtu.edu&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should first make sure you have the selected pins connected to your PC. For example, for FreeMASTER over LPUART, if you only have the USB cable from the EVB to the PC and nothing else, you will not be able to communicate with it. The pins that are used for the USB are PTC6 and PTC7, from LPUART1 instance. You should check out the&amp;nbsp;quick start guide (&lt;A href="https://www.nxp.com/docs/en/quick-reference-guide/S32K144EVB-QSG.pdf"&gt;here&lt;/A&gt;). In every peripheral configuration block you should make sure the pins are correctly selected. You can find examples for FreeMASTER and CAN in our example library (that comes installed with the toolbox).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110713i7F4096E8FC163404/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 08:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1057699#M4502</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2020-08-26T08:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1152960#M5024</link>
      <description>&lt;P&gt;Hi Razvan,&lt;/P&gt;&lt;P&gt;I have done the configuration. But still not able to connect to freeMaster.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please find the attached dummy model. Can you please let me know what is possibly going wrong?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rubeena&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Sep 2020 15:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1152960#M5024</guid>
      <dc:creator>parveez</dc:creator>
      <dc:date>2020-09-14T15:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1153055#M5026</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/112879"&gt;@parveez&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I had a look on your model and there are multiple reasons for its behaviour.&lt;/P&gt;
&lt;P&gt;If I understand correctly, you want to connect with FreeMaster over the USB cable/Serial connection and to transfer messages over CAN bus.&lt;/P&gt;
&lt;P&gt;If so, this is what I've found in the attached model.&lt;/P&gt;
&lt;P&gt;1. FreeMaster setup: Razvan mentioned above the pins required for the connection. For the FreeMaster you have selected other pins that the ones connected to OpenSDA.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mariuslucianand_0-1600117914068.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/125108iBBE88CD9CB76421A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mariuslucianand_0-1600117914068.png" alt="mariuslucianand_0-1600117914068.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mariuslucianand_0-1600117914068.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;2. The FCAN_Receive block makes some settings in the step function, configuring the RX message buffer. And in the model that you send, the code generated by the Receive block was inserted before the FCAN Configuration code, which means that the board was ending up running a dummy handler. To set the execution order for some important blocks, like the Config, Send and Receive, you can right click on the block, open the Properties and insert a priority.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mariuslucianand_2-1600118702289.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/125110iC40325D4F6075F2D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mariuslucianand_2-1600118702289.png" alt="mariuslucianand_2-1600118702289.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mariuslucianand_2-1600118702289.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Finally the execution order looks like this: First is the FCAN COnfig, then the Transmit and then the receive.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mariuslucianand_1-1600118669995.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/125109iAF147C34F34382AE/image-size/large?v=v2&amp;amp;px=999" role="button" title="mariuslucianand_1-1600118669995.png" alt="mariuslucianand_1-1600118669995.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mariuslucianand_1-1600118669995.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Last but not least, are you powering the board externally using the J16 connector? because as far as I know, in order to use the CAN transciever, you need to power the board using the external supply.&lt;/P&gt;
&lt;P&gt;I can't test the communication because I don't have for now a CAN analyzer but the FreeMaster over USB works.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Sep 2020 21:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1153055#M5026</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2020-09-14T21:27:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1164583#M5118</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;This solution worked for me with one controller. But something went wrong with the controller and I was not able to fix it. So I purchased a new controller, now I am not able to verify CAN communication. I used Vector CANAlyzer but I do not see any communication. I have 12V connected to the board and Pin J107 (1-2) are also connected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please help me what else I can do?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the problem I had with my old controller and was not able to fix: &lt;FONT&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K144-not-working/m-p/1160684" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K/S32K144-not-working/m-p/1160684&lt;/A&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 14:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1164583#M5118</guid>
      <dc:creator>parveez</dc:creator>
      <dc:date>2020-10-08T14:44:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1167188#M5143</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179060"&gt;@Elson_Sarah&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Can you provide more details? Do you have the same exact model? Have you tried to rearrange the CAN blocks?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 06:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1167188#M5143</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2020-10-14T06:27:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 EVB CAN Communication using MBD</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1495748#M7547</link>
      <description>&lt;P&gt;Is it possible to use Freemaster on CAN, and use the CAN Tx &amp;amp; Rx blocks on the same bus, from within Simulink ?&lt;/P&gt;&lt;P&gt;(our target ECU has no usb/uart interface - just CAN). I am using v4.2 of the MBDT&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 17:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k144-EVB-CAN-Communication-using-MBD/m-p/1495748#M7547</guid>
      <dc:creator>gmud1234</dc:creator>
      <dc:date>2022-07-26T17:14:40Z</dc:date>
    </item>
  </channel>
</rss>