<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K PIL in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-PIL/m-p/1153790#M5046</link>
    <description>&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;I am trying to run PIL with S32K board and Simulink. I just want to run a function that takes 300 inputs and produce 100 outputs in double format. My objective is to benchmark the performance of the processor running this algorithm in the loop. My question is do NXP support this with Simulink ? and do I need extra components besides the S32K board i.e., connections or any other?.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 16 Sep 2020 03:02:42 GMT</pubDate>
    <dc:creator>MinaNaguib</dc:creator>
    <dc:date>2020-09-16T03:02:42Z</dc:date>
    <item>
      <title>S32K PIL</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-PIL/m-p/1153790#M5046</link>
      <description>&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P&gt;I am trying to run PIL with S32K board and Simulink. I just want to run a function that takes 300 inputs and produce 100 outputs in double format. My objective is to benchmark the performance of the processor running this algorithm in the loop. My question is do NXP support this with Simulink ? and do I need extra components besides the S32K board i.e., connections or any other?.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Sep 2020 03:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-PIL/m-p/1153790#M5046</guid>
      <dc:creator>MinaNaguib</dc:creator>
      <dc:date>2020-09-16T03:02:42Z</dc:date>
    </item>
    <item>
      <title>Re: S32K PIL</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-PIL/m-p/1156880#M5071</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178025"&gt;@MinaNaguib&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Yes, NXP supports running PIL on the S32K1xx board. We also provide some PIL example in our toolbox so I think they are a good starting point.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2020 10:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-PIL/m-p/1156880#M5071</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2020-09-22T10:42:21Z</dc:date>
    </item>
  </channel>
</rss>