<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Issue with FTM Input Edge Capture Block in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-FTM-Input-Edge-Capture-Block/m-p/1078165#M4680</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mariuslucianandrei"&gt;mariuslucianandrei&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help, it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Utku Çekmegül&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2020 11:57:29 GMT</pubDate>
    <dc:creator>utkuckmgl</dc:creator>
    <dc:date>2020-07-22T11:57:29Z</dc:date>
    <item>
      <title>Issue with FTM Input Edge Capture Block</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-FTM-Input-Edge-Capture-Block/m-p/1078163#M4678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using FTM blocks in my design but I can not simulate or build model when I use FTM Input Edge Capture block. Only this block give me errors. Can you please help me to solve this problem ?&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116575i009F5B86DE400410/image-size/large?v=v2&amp;amp;px=999" title="BeforeError.PNG" alt="BeforeError.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;There is no errors in this model.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116579iFB7F6DC6FDA59F42/image-size/large?v=v2&amp;amp;px=999" title="AfterError.PNG" alt="AfterError.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have this errors with addition of FTM Input Edge Capture block.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;Utku Çekmegül&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 11:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-FTM-Input-Edge-Capture-Block/m-p/1078163#M4678</guid>
      <dc:creator>utkuckmgl</dc:creator>
      <dc:date>2020-07-22T11:24:08Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with FTM Input Edge Capture Block</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-FTM-Input-Edge-Capture-Block/m-p/1078164#M4679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/utkuckmgl@gmail.com"&gt;utkuckmgl@gmail.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason that this error is caused is related to the fact that you are trying to use the same FTM module, 4 same as input and&amp;nbsp;PWM generator which is not possible in hardware.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116578i880164EAF6675836/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The FTM module uses the counter in a different way for PWM generation than for FTM Input Edge Capture. Please select other FTM Module for FTM Input Edge than the module 4 and look after an appropriate PIN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Marius&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 11:34:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-FTM-Input-Edge-Capture-Block/m-p/1078164#M4679</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2020-07-22T11:34:29Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with FTM Input Edge Capture Block</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-FTM-Input-Edge-Capture-Block/m-p/1078165#M4680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mariuslucianandrei"&gt;mariuslucianandrei&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help, it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Utku Çekmegül&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 11:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-FTM-Input-Edge-Capture-Block/m-p/1078165#M4680</guid>
      <dc:creator>utkuckmgl</dc:creator>
      <dc:date>2020-07-22T11:57:29Z</dc:date>
    </item>
  </channel>
</rss>