<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: S32K144EVB not recognised by USB after 2+ hours of correct behaviour</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070302#M4616</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marius,&lt;/P&gt;&lt;P&gt;I was able to spend some time on a Zoom call showing the board lack of USB power-up to Mark Dunnett (ex-Motorola/Freescale/NXP) and the fact that the reset button does not allow the board to go into bootloader mode. I have shipped the card to him so that he can revive it with a JTAG (or similar) debugger. Mark felt it might be a faulty reset button (constantly resetting the board - possible but statistically not so likely) or the code in the debug chip becoming corrupted. I think the situation could be clearer once he connects with a Segger.&lt;/P&gt;&lt;P&gt;Thank you for the support so far, I will report once I know more :-)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jun 2020 13:15:02 GMT</pubDate>
    <dc:creator>chrisc1</dc:creator>
    <dc:date>2020-06-10T13:15:02Z</dc:date>
    <item>
      <title>S32K144EVB not recognised by USB after 2+ hours of correct behaviour</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070298#M4612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I received our S32K144EVB today and managed to get approximately 5 builds on to it. It came up as a drive (although the name wasn’t recognised, it was just as E: drive). I flashed a couple of builds via Simulink to use the buttons and LED’s blinking at different frequencies, then played with a couple to manipulate signals via the rotary pot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now the board takes approx. 60 to 180 seconds to illuminate its status LEDs when I plug it into USB. It’s as if the driver does not respond like it did when I first plugged in. Often it doesn’t even come to life.&lt;/P&gt;&lt;P&gt;Also, I can no longer see the drive in Windows 10. However I know that it still has a valid application because the switches and LEDs still do what the last build was for. Therefore I can’t drag and drop *.mot files.&lt;/P&gt;&lt;P&gt;I tried connecting with FreeMASTER and the ToolsàWizard only shows me COM1, but no longer shows me what was COM3 for OpenSDA.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I looked through the forums for various articles and came across these:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/488831"&gt;https://community.nxp.com/thread/488831&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/464233"&gt;https://community.nxp.com/thread/464233&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/486976"&gt;https://community.nxp.com/thread/486976&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The board was ordered from Farnell, came from USA and with lot AOIF192502 and I used the latest and greatest MBDT to create the builds. I can postulate that “maybe” some aspect of Windows 10 on my workstation might be causing USB driver issues with OpenSDA but I would appreciate if anyone has some pragmatic checks to suggest. All other phones and USB sticks and drive work ok. In fact I had the same issue when plugging into a laptop: board not recognised.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don’t yet have the right cable to give the board independent power but anyway I don’t feel that would help me with USB detection. I am curious as to why the board worked and then now it does not. It’s not an issue with ports, I’ve tried every single one of the 8 I have available. I don’t have the small enough probes right now to access test points on the PCB to check for supply voltage. I’ve had issues in the past with USB drivers when I used to support Motorsport data-loggers but not had this kind of issue before where a PCB behaves dead 80% of the time after 2.5 hours of usage. Any ideas?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Chris Catto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2020 21:10:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070298#M4612</guid>
      <dc:creator>chrisc1</dc:creator>
      <dc:date>2020-06-08T21:10:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB not recognised by USB after 2+ hours of correct behaviour</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070299#M4613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/chrisc@rmlgroup.com"&gt;chrisc@rmlgroup.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Indeed you are facing a strange behavior of the board. But, from the detailed explanation, I assume that the controller is fine, but there is an issue with the OpenSDA.&lt;/P&gt;&lt;P&gt;If I had&amp;nbsp;these issues, I would try the following approaches:&lt;/P&gt;&lt;P&gt;1. Install the PEDrivers. Go&amp;nbsp;to&amp;nbsp;&lt;A class="link-titled" href="http://www.pemicro.com/opensda/" title="http://www.pemicro.com/opensda/"&gt;PEmicro | Experts in Embedded tools for Flash Programming and Development&lt;/A&gt;&amp;nbsp; and under Windows USB Drivers there is the PEDrivers_install.exe. Please install the driver and check the board behavior.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/112398i55E9BB0221A3754B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2. If the driver installation does not solve the issue, then I would try reprogramming the OpenSDA drive, and this can be also a good thing to be sure that it runs the latest firmware: V1.19.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/112399i86F6BD7AFDB7B2A7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is a very simple process: Go to the same PEMicro page, and download the Firmware Apps. In the archive locate the&amp;nbsp;&lt;STRONG&gt;MSD-DEBUG-EVB-S32K144_Pemicro_v119.SDA &lt;/STRONG&gt;file and extract it on your PC. On the S32K144 Board, change the J104 (the one next to the USB socket) to the 1-2 position. Unplug the board and while you&amp;nbsp;are holding the RESET button pressed, plug in the board. A new BOOTLOADER drive should be mounted. Now copy the .SDA file to the new bootloader. When finished uplung and reconnect again the board. Don't forget to set the J104 to 2-3 position. You cand find more about this process in this User Guide&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/OPENSDAUG.pdf" title="https://www.nxp.com/docs/en/user-guide/OPENSDAUG.pdf"&gt;https://www.nxp.com/docs/en/user-guide/OPENSDAUG.pdf&lt;/A&gt;&amp;nbsp;&amp;nbsp;chapter 2.1 and 2.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let's see if this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Marius&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2020 20:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070299#M4613</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2020-06-09T20:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB not recognised by USB after 2+ hours of correct behaviour</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070300#M4614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Marius,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ok so after installing the PE Micro drivers on the PC I was stuck because the board was not actually turning on (status LEDs showing life). I tried a few reboots of the two PCs and no joy. Tried another laptop and its USB, no change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, leaving USB aside, I'm thinking of using the power feed into J16. The Quickstart guide notes that it accepts 5V to 12V. I've used this power adaptor:&amp;nbsp;&lt;A class="link-titled" href="https://richelectronics.co.uk/product/oem-adapter-ads0126a-x120100-100-240vacin-12vdc-1-0a-out-ee-brightbox-etc-ol0691" title="https://richelectronics.co.uk/product/oem-adapter-ads0126a-x120100-100-240vacin-12vdc-1-0a-out-ee-brightbox-etc-ol0691"&gt;OEM Adapter ADS0126A-X120100 100-240VACin 12VDC 1.0A out EE Brightbox etc OL0691 | Rich Electronics&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board powers up correctly once I have J107 set to 1&amp;amp;2. So it looks like the internal power circuitry is intact.&lt;/P&gt;&lt;P&gt;Still not recognised via USB so I'm guessing I will have to do the driver update etc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 09:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070300#M4614</guid>
      <dc:creator>chrisc1</dc:creator>
      <dc:date>2020-06-10T09:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB not recognised by USB after 2+ hours of correct behaviour</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070301#M4615</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/137779"&gt;@chrisc1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please perform the Open SDA firmware update.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 08:00:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070301#M4615</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-03-24T08:00:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB not recognised by USB after 2+ hours of correct behaviour</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070302#M4616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marius,&lt;/P&gt;&lt;P&gt;I was able to spend some time on a Zoom call showing the board lack of USB power-up to Mark Dunnett (ex-Motorola/Freescale/NXP) and the fact that the reset button does not allow the board to go into bootloader mode. I have shipped the card to him so that he can revive it with a JTAG (or similar) debugger. Mark felt it might be a faulty reset button (constantly resetting the board - possible but statistically not so likely) or the code in the debug chip becoming corrupted. I think the situation could be clearer once he connects with a Segger.&lt;/P&gt;&lt;P&gt;Thank you for the support so far, I will report once I know more :-)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 13:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070302#M4616</guid>
      <dc:creator>chrisc1</dc:creator>
      <dc:date>2020-06-10T13:15:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB not recognised by USB after 2+ hours of correct behaviour</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070303#M4617</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/137779"&gt;@chrisc1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Mark felt it might be a faulty reset button (constantly resetting the board - possible but statistically not so likely)&lt;/SPAN&gt;&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Was the RED LED next to the reset button constantly turned on?&lt;/P&gt;
&lt;P&gt;Because in this case, the&amp;nbsp;P&amp;amp;E Recovery Utility works great on S32K144 too. Find more info here:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A class="link-titled" title="https://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-low-power/" href="https://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-low-power/" target="_blank"&gt;Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 08:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K144EVB-not-recognised-by-USB-after-2-hours-of-correct/m-p/1070303#M4617</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2021-03-24T08:00:45Z</dc:date>
    </item>
  </channel>
</rss>