<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: can I use the FOC code developed by NXP for the Linux motor to control another type of motor in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057684#M4495</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/abderrahimjamaoui@gmail.com"&gt;abderrahimjamaoui@gmail.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;In general, if you only change the motor (i.e. Linix motor with another type of PMSM surface mount motor), you do not have to change the algorithm but you need to update the parameters of the motor and/or sensors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, you need to retune the PI controllers for the new motor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are considered to be parameters for the FOC hence we can say that C-code does not change but the Data needs to be updated to have the motor running correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jun 2020 06:05:11 GMT</pubDate>
    <dc:creator>Daniel_Popa</dc:creator>
    <dc:date>2020-06-11T06:05:11Z</dc:date>
    <item>
      <title>can I use the FOC code developed by NXP for the Linux motor to control another type of motor</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057681#M4492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning all,&lt;BR /&gt;I have a question, please. I am working on brushless motor control and want to know if I can use the FOC code developed by NXP for the Linux motor to control another type of motor. do I have to modify the code to adapt it with my motor or is it a general code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 11:24:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057681#M4492</guid>
      <dc:creator>abderrahimjamao</dc:creator>
      <dc:date>2020-06-04T11:24:09Z</dc:date>
    </item>
    <item>
      <title>Re: can I use the FOC code developed by NXP for the Linux motor to control another type of motor</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057682#M4493</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/abderrahimjamaoui@gmail.com"&gt;abderrahimjamaoui@gmail.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if you are referring to our models or other NXP code -- on this community we mainly handle topics regarding MATLAB/Simulink and our toolboxes. If you have specific questions regarding the examples we ship for FOC, &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/adriantudor"&gt;adriantudor&lt;/A&gt;‌ can help with some answers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 07:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057682#M4493</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2020-06-10T07:58:52Z</dc:date>
    </item>
    <item>
      <title>Re: can I use the FOC code developed by NXP for the Linux motor to control another type of motor</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057683#M4494</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I'm sorry to ask the question in this community.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 08:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057683#M4494</guid>
      <dc:creator>abderrahimjamao</dc:creator>
      <dc:date>2020-06-10T08:41:43Z</dc:date>
    </item>
    <item>
      <title>Re: can I use the FOC code developed by NXP for the Linux motor to control another type of motor</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057684#M4495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/abderrahimjamaoui@gmail.com"&gt;abderrahimjamaoui@gmail.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;In general, if you only change the motor (i.e. Linix motor with another type of PMSM surface mount motor), you do not have to change the algorithm but you need to update the parameters of the motor and/or sensors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, you need to retune the PI controllers for the new motor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are considered to be parameters for the FOC hence we can say that C-code does not change but the Data needs to be updated to have the motor running correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 06:05:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057684#M4495</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2020-06-11T06:05:11Z</dc:date>
    </item>
    <item>
      <title>Re: can I use the FOC code developed by NXP for the Linux motor to control another type of motor</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057685#M4496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ok, thank you so much. I don't understand how to retune the PI controllers for my motor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 08:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/can-I-use-the-FOC-code-developed-by-NXP-for-the-Linux-motor-to/m-p/1057685#M4496</guid>
      <dc:creator>abderrahimjamao</dc:creator>
      <dc:date>2020-06-11T08:40:23Z</dc:date>
    </item>
  </channel>
</rss>