<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Quicker code generation using the MBD Toolbox 3.2.0 in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Quicker-code-generation-using-the-MBD-Toolbox-3-2-0/m-p/1055551#M4475</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/constantinrazvan.chivu"&gt;constantinrazvan.chivu&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I would appreciate very much is you can share these modifications with me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards, Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Aug 2020 12:01:57 GMT</pubDate>
    <dc:creator>rafael_barbosa</dc:creator>
    <dc:date>2020-08-24T12:01:57Z</dc:date>
    <item>
      <title>Quicker code generation using the MBD Toolbox 3.2.0</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Quicker-code-generation-using-the-MBD-Toolbox-3-2-0/m-p/1055549#M4473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I notice after updating the MBD toolbox from the version 3.0.0 to the newest version 3.2.0 that the code generation is slower that usual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I disable some callbacks in order to make it quicker?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, how can I stop the "mbd_mpc_consistency_checks(bdroot(gcs));" callback to load automatically?&amp;nbsp;&lt;/P&gt;&lt;P&gt;(I try to delete it, but It loads automatically after building the model)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109137i2061AAC06B0D9508/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards, Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2020 12:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Quicker-code-generation-using-the-MBD-Toolbox-3-2-0/m-p/1055549#M4473</guid>
      <dc:creator>rafael_barbosa</dc:creator>
      <dc:date>2020-08-21T12:03:23Z</dc:date>
    </item>
    <item>
      <title>Re: Quicker code generation using the MBD Toolbox 3.2.0</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Quicker-code-generation-using-the-MBD-Toolbox-3-2-0/m-p/1055550#M4474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rafael.barbosa@chassisbrakes.com"&gt;rafael.barbosa@chassisbrakes.com&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The consistency checks are set from 2 scripts (2 different scenarios) - so you'll have to edit both of them. The scripts I'm talking about are the following:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;mbd_mpc_set_tmf&lt;/P&gt;&lt;P&gt;mbd_mpc_model_init_fcn&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem with these scripts is that they are pcoded - so you can't edit them as they are. If you are sure you don't need the consistency checks, I can edit them for you and attach them here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the code generation, in the newer versions of our toolboxes we have added more functionality, more checks, etc. and this lead to a slow-down on code generation speed. There might be room for improvement, but unfortunately for the moment we are focused on other toolboxes so we can not investigate this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Razvan.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2020 15:20:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Quicker-code-generation-using-the-MBD-Toolbox-3-2-0/m-p/1055550#M4474</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2020-08-21T15:20:09Z</dc:date>
    </item>
    <item>
      <title>Re: Quicker code generation using the MBD Toolbox 3.2.0</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Quicker-code-generation-using-the-MBD-Toolbox-3-2-0/m-p/1055551#M4475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/constantinrazvan.chivu"&gt;constantinrazvan.chivu&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I would appreciate very much is you can share these modifications with me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards, Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2020 12:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Quicker-code-generation-using-the-MBD-Toolbox-3-2-0/m-p/1055551#M4475</guid>
      <dc:creator>rafael_barbosa</dc:creator>
      <dc:date>2020-08-24T12:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: Quicker code generation using the MBD Toolbox 3.2.0</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Quicker-code-generation-using-the-MBD-Toolbox-3-2-0/m-p/1055552#M4476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rafael.barbosa@chassisbrakes.com"&gt;rafael.barbosa@chassisbrakes.com&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here you go - I have attached the 2 files here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find them in the following paths:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;{ROOT}\mbdtbx_mpc\mscripts\config&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;{ROOT}\&lt;/SPAN&gt;mbdtbx_mpc\mscripts\model&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2020 15:07:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Quicker-code-generation-using-the-MBD-Toolbox-3-2-0/m-p/1055552#M4476</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2020-08-24T15:07:06Z</dc:date>
    </item>
  </channel>
</rss>