<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with CAN interface when using eTimer in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055179#M4466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am using the MBD toolbox 3.0.0 and the target micro-controller is MPC5744P. For the problem that I bring here, I am also using the PMIC&amp;nbsp;35FS6500.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;My target is to use the etimer0 as a counter to measure the time between two interruptions and exchange CAN data in parallel.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I can send and receive CAN messages in the attached example when I delete (or comment out) the eTimer related blocks:&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109327i2D74A11FB0156E04/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;However when I include these eTimer related blocks in the model, the can messages does not works anymore in the target microcontroller.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Why is it happening?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mariuslucianandrei"&gt;mariuslucianandrei&lt;/A&gt;‌&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am using Canoe 11.0 from vector to exchange messages with the target microcontroller.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Kind Regards, Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Aug 2020 10:26:40 GMT</pubDate>
    <dc:creator>rafael_barbosa</dc:creator>
    <dc:date>2020-08-03T10:26:40Z</dc:date>
    <item>
      <title>Problem with CAN interface when using eTimer</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055179#M4466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am using the MBD toolbox 3.0.0 and the target micro-controller is MPC5744P. For the problem that I bring here, I am also using the PMIC&amp;nbsp;35FS6500.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;My target is to use the etimer0 as a counter to measure the time between two interruptions and exchange CAN data in parallel.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I can send and receive CAN messages in the attached example when I delete (or comment out) the eTimer related blocks:&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/109327i2D74A11FB0156E04/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;However when I include these eTimer related blocks in the model, the can messages does not works anymore in the target microcontroller.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Why is it happening?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mariuslucianandrei"&gt;mariuslucianandrei&lt;/A&gt;‌&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am using Canoe 11.0 from vector to exchange messages with the target microcontroller.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Kind Regards, Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2020 10:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055179#M4466</guid>
      <dc:creator>rafael_barbosa</dc:creator>
      <dc:date>2020-08-03T10:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with CAN interface when using eTimer</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055180#M4467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rafael.barbosa@chassisbrakes.com"&gt;rafael.barbosa@chassisbrakes.com&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First of all consider installing our latest version of MPC toolbox (&lt;A href="https://community.nxp.com/docs/DOC-346265"&gt;https://community.nxp.com/docs/DOC-346265&lt;/A&gt;&amp;nbsp;) - the support for earlier versions will be limited.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your issue, I have a few questions: are you using a shared pin between eTimer and CAN? If yes, that would be a problem with our consistency check, as it should have warned you. Next, do you know if the application is still working after adding the eTimer blocks? Do you have a blinking LED or something to let you know? Or if you have put the executable in the debugger and saw the application is running normally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2020 07:00:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055180#M4467</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2020-08-05T07:00:56Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with CAN interface when using eTimer</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055181#M4468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/constantinrazvan.chivu"&gt;constantinrazvan.chivu&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Indeed I am considering to update the toolbox for the version 3.2.0. It will be performed as soon as I reach the next project baseline. Thank you for point it out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No shared pins between the modules:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PMIC pins for SPI: PTC7, PTC6, PTC5 and PTF3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAN1 pins: PTA15, PTA14, PTD3 and PTD4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;eTimer&amp;nbsp;pin: PTC14&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After adding the eTimer blocks the application runs. I am using the debugger (PE Micro).&lt;/P&gt;&lt;P&gt;I am intrigued what is going on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards, Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2020 07:10:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055181#M4468</guid>
      <dc:creator>rafael_barbosa</dc:creator>
      <dc:date>2020-08-06T07:10:20Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with CAN interface when using eTimer</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055182#M4469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/constantinrazvan.chivu"&gt;constantinrazvan.chivu&lt;/A&gt;‌ and &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mariuslucianandrei"&gt;mariuslucianandrei&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have some updating regarding this topic?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards, Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 08:04:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055182#M4469</guid>
      <dc:creator>rafael_barbosa</dc:creator>
      <dc:date>2020-08-12T08:04:41Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with CAN interface when using eTimer</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055183#M4470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rafael.barbosa@chassisbrakes.com"&gt;rafael.barbosa@chassisbrakes.com&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately due to our current workload it is hard to check this issue, given that it is in a version this old. Can you please check if you replicate this issue in the latest version? If the answer would be yes, we could give you a solution quicker for the v3.2.0 (than the v3.0.0).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 08:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055183#M4470</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2020-08-12T08:22:58Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with CAN interface when using eTimer</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055184#M4471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/constantinrazvan.chivu"&gt;constantinrazvan.chivu&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the installation of the new version v3.2.0 this issue was solved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The clock configuration updating&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110113iE7E9D256114B6C69/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;on the new toolbox version fixed the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards, Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 11:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055184#M4471</guid>
      <dc:creator>rafael_barbosa</dc:creator>
      <dc:date>2020-08-12T11:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with CAN interface when using eTimer</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055185#M4472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rafael.barbosa@chassisbrakes.com"&gt;rafael.barbosa@chassisbrakes.com&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for confirming this!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2020 13:15:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-with-CAN-interface-when-using-eTimer/m-p/1055185#M4472</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2020-08-19T13:15:28Z</dc:date>
    </item>
  </channel>
</rss>