<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Pil Mode on KV3x in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Re-Pil-Mode-on-KV3x/m-p/972136#M3813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/pbgemann001@ikasle.ehu.eus"&gt;pbgemann001@ikasle.ehu.eus&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for answering so late, but we were working on MBDT for S32K 4.0.1 release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Right now the PIL is not working using the GCC compiler, somehow the application crashes on the board. I mentioned that here &lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/501745#comment" title="https://community.nxp.com/message/1145564#comment-1162694"&gt;https://community.nxp.com/message/1145564#comment-1162694&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to fix this issue the next week.&lt;/P&gt;&lt;P&gt;Can you try to run PIL simulation using the IAR compiler?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jul 2019 13:40:58 GMT</pubDate>
    <dc:creator>paulvlase</dc:creator>
    <dc:date>2019-07-26T13:40:58Z</dc:date>
    <item>
      <title>Re: Pil Mode on KV3x</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Re-Pil-Mode-on-KV3x/m-p/972135#M3812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/paulvlase"&gt;paulvlase&lt;/A&gt;,&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;another problem occured. After setting up on another PC everything except the PIL works. I get the following error&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="PILfail.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90122i47B650191ABC62C1/image-size/large?v=v2&amp;amp;px=999" role="button" title="PILfail.PNG" alt="PILfail.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I am using the same model, Matlabversion and DevBoard as before.&lt;/P&gt;&lt;P&gt;I will attach the slprj and the diagnostics output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess it has to do with the location of files again? I have installed Matlab in D instead C on this PC could that be the cause?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2019 09:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Re-Pil-Mode-on-KV3x/m-p/972135#M3812</guid>
      <dc:creator>pbgemann001</dc:creator>
      <dc:date>2019-07-02T09:50:21Z</dc:date>
    </item>
    <item>
      <title>Re: Pil Mode on KV3x</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Re-Pil-Mode-on-KV3x/m-p/972136#M3813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/pbgemann001@ikasle.ehu.eus"&gt;pbgemann001@ikasle.ehu.eus&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for answering so late, but we were working on MBDT for S32K 4.0.1 release.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Right now the PIL is not working using the GCC compiler, somehow the application crashes on the board. I mentioned that here &lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/501745#comment" title="https://community.nxp.com/message/1145564#comment-1162694"&gt;https://community.nxp.com/message/1145564#comment-1162694&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to fix this issue the next week.&lt;/P&gt;&lt;P&gt;Can you try to run PIL simulation using the IAR compiler?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2019 13:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Re-Pil-Mode-on-KV3x/m-p/972136#M3813</guid>
      <dc:creator>paulvlase</dc:creator>
      <dc:date>2019-07-26T13:40:58Z</dc:date>
    </item>
  </channel>
</rss>