<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックMPC5643xL: Return to default flash configuration</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5643xL-Return-to-default-flash-configuration/m-p/971584#M3802</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif; color: black; background: white;"&gt;I have an issue with the flash configuration of a MPC5643L. &lt;BR /&gt; I think that I have overwritten boot registers or something like that because when I try to download an .elf file into the flash memory it works properly (I can see a CAN message). But after a power-off cycle,&amp;nbsp;the application doesn’t restart because I cannot see the CAN message anymore. &lt;BR /&gt; Could you please let me know the procedure to go back to the default configuration of the flash? &lt;BR /&gt; &lt;BR /&gt; Thanks in advance, &lt;BR /&gt; Borja&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Oct 2019 06:43:06 GMT</pubDate>
    <dc:creator>borja_heriz</dc:creator>
    <dc:date>2019-10-28T06:43:06Z</dc:date>
    <item>
      <title>MPC5643xL: Return to default flash configuration</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5643xL-Return-to-default-flash-configuration/m-p/971584#M3802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial',sans-serif; color: black; background: white;"&gt;I have an issue with the flash configuration of a MPC5643L. &lt;BR /&gt; I think that I have overwritten boot registers or something like that because when I try to download an .elf file into the flash memory it works properly (I can see a CAN message). But after a power-off cycle,&amp;nbsp;the application doesn’t restart because I cannot see the CAN message anymore. &lt;BR /&gt; Could you please let me know the procedure to go back to the default configuration of the flash? &lt;BR /&gt; &lt;BR /&gt; Thanks in advance, &lt;BR /&gt; Borja&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2019 06:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5643xL-Return-to-default-flash-configuration/m-p/971584#M3802</guid>
      <dc:creator>borja_heriz</dc:creator>
      <dc:date>2019-10-28T06:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643xL: Return to default flash configuration</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5643xL-Return-to-default-flash-configuration/m-p/971585#M3803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/borja.heriz@tecnalia.com"&gt;borja.heriz@tecnalia.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, If I understand correctly you are using the RappId Bootloader to download the code over CAN and the application is working correctly until restart. Are you sure that you have selected the flash and not the ram for target memory? What Matlab version are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marius&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2019 09:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5643xL-Return-to-default-flash-configuration/m-p/971585#M3803</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2019-10-29T09:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5643xL: Return to default flash configuration</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5643xL-Return-to-default-flash-configuration/m-p/971586#M3804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Marius-lucian Andrei,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;No, I just jtagged the elf using S32 IDE.&amp;nbsp;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;And yes, I'm sure that I've selected FLASH option as target memory.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Any clue about what could be happening?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Borja&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2019 22:28:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5643xL-Return-to-default-flash-configuration/m-p/971586#M3804</guid>
      <dc:creator>borja_heriz</dc:creator>
      <dc:date>2019-10-31T22:28:28Z</dc:date>
    </item>
  </channel>
</rss>