<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックVDS currents are higher than expected (MW7IC930N)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/VDS-currents-are-higher-than-expected-MW7IC930N/m-p/945283#M3568</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm currently working on a prototype power amp using the MW7IC930N. In my ADS simulation, I used 28V for VDS1 and VDS2, and 3.16V and 2.922V for VGS1 and VGS2 respectively to get optimum performance (Gain = 35dB). The current consumption is 106mA and 286mA for VDS1 and VDS2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However when I used the same voltages in my actual setup I'm getting a combined current of 1.1A (I'm using a single 28V supply for VDS1 and VDS2) and only a gain of 20-21 dB. Is there something that I could be missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made sure that my pcb is properly grounded and that the IC has a proper heatsink below it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jul 2019 09:09:32 GMT</pubDate>
    <dc:creator>jason_hipolito</dc:creator>
    <dc:date>2019-07-05T09:09:32Z</dc:date>
    <item>
      <title>VDS currents are higher than expected (MW7IC930N)</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/VDS-currents-are-higher-than-expected-MW7IC930N/m-p/945283#M3568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm currently working on a prototype power amp using the MW7IC930N. In my ADS simulation, I used 28V for VDS1 and VDS2, and 3.16V and 2.922V for VGS1 and VGS2 respectively to get optimum performance (Gain = 35dB). The current consumption is 106mA and 286mA for VDS1 and VDS2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However when I used the same voltages in my actual setup I'm getting a combined current of 1.1A (I'm using a single 28V supply for VDS1 and VDS2) and only a gain of 20-21 dB. Is there something that I could be missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made sure that my pcb is properly grounded and that the IC has a proper heatsink below it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 09:09:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/VDS-currents-are-higher-than-expected-MW7IC930N/m-p/945283#M3568</guid>
      <dc:creator>jason_hipolito</dc:creator>
      <dc:date>2019-07-05T09:09:32Z</dc:date>
    </item>
    <item>
      <title>Re: VDS currents are higher than expected (MW7IC930N)</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/VDS-currents-are-higher-than-expected-MW7IC930N/m-p/945284#M3569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jason.hipolito@entropysolution.com"&gt;jason.hipolito@entropysolution.com&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not want to disappoint you but this community is related with MATLAB/Simulink Model Based Design Toolbox issues.&lt;/P&gt;&lt;P&gt;I think it would be better if you could post your questing into RF related communities like:&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/community/other/content?filterID=contentstatus[published]~category[rf]"&gt;https://community.nxp.com/community/other/content?filterID=contentstatus[published]~category[rf]&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 09:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/VDS-currents-are-higher-than-expected-MW7IC930N/m-p/945284#M3569</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2019-07-05T09:35:31Z</dc:date>
    </item>
  </channel>
</rss>