<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: Build Error because of S32 Design Studio for Power (MBD Tool MPC57xx)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Error-because-of-S32-Design-Studio-for-Power-MBD-Tool/m-p/933919#M3472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/abhishek.kumar@chassisbrakes.com"&gt;abhishek.kumar@chassisbrakes.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are some differences in the folder structure, between the S32DS for PA 2.1 vs 2017.R1, so, in order to build using the compiler from S32DS V2.1, the following changes must be performed:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;1.&amp;nbsp;S32DS_PA_TOOL must be set as path variable as 'C:\NXP\S32DS_Power_v2.1'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;2. the .tmf file from&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;src\mbdtbx_mpc574x\mbdtbx_mpc574x location must be updated with the one attach.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Marius&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Oct 2019 21:35:37 GMT</pubDate>
    <dc:creator>mariuslucianand</dc:creator>
    <dc:date>2019-10-01T21:35:37Z</dc:date>
    <item>
      <title>Build Error because of S32 Design Studio for Power (MBD Tool MPC57xx)</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Error-because-of-S32-Design-Studio-for-Power-MBD-Tool/m-p/933918#M3471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have MATLAB 2018b.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I installed Design Studio for Power 2.1 and suddenly Simulink file do not build anymore&amp;nbsp;&lt;/P&gt;&lt;P&gt;I changed the registry value (below)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88030i4BB8C55273553DB4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I have attached the error and build file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mariuslucianandrei"&gt;mariuslucianandrei&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 11:32:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Error-because-of-S32-Design-Studio-for-Power-MBD-Tool/m-p/933918#M3471</guid>
      <dc:creator>abhishek_kumar1</dc:creator>
      <dc:date>2019-10-01T11:32:39Z</dc:date>
    </item>
    <item>
      <title>Re: Build Error because of S32 Design Studio for Power (MBD Tool MPC57xx)</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Error-because-of-S32-Design-Studio-for-Power-MBD-Tool/m-p/933919#M3472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/abhishek.kumar@chassisbrakes.com"&gt;abhishek.kumar@chassisbrakes.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are some differences in the folder structure, between the S32DS for PA 2.1 vs 2017.R1, so, in order to build using the compiler from S32DS V2.1, the following changes must be performed:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;1.&amp;nbsp;S32DS_PA_TOOL must be set as path variable as 'C:\NXP\S32DS_Power_v2.1'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;2. the .tmf file from&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;src\mbdtbx_mpc574x\mbdtbx_mpc574x location must be updated with the one attach.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Marius&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 21:35:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Error-because-of-S32-Design-Studio-for-Power-MBD-Tool/m-p/933919#M3472</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2019-10-01T21:35:37Z</dc:date>
    </item>
  </channel>
</rss>