<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: Error with MBDT for 9s12zvc？？？？？</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Error-with-MBDT-for-9s12zvc/m-p/919330#M3363</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi community;&lt;/P&gt;&lt;P&gt;The problem has been found to be a solution. as follows:&lt;BR /&gt;1. Follow this step to repair the .c file with the following address: "https://community.nxp.com/thread/450789";&lt;BR /&gt;2, mbd_s12zvc_block_mscan0_check.p file can not be directly modified to .none, you need to use the following attachment to replace;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jun 2019 08:06:56 GMT</pubDate>
    <dc:creator>xuxingwen0719</dc:creator>
    <dc:date>2019-06-14T08:06:56Z</dc:date>
    <item>
      <title>Error with MBDT for 9s12zvc？？？？？</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Error-with-MBDT-for-9s12zvc/m-p/919329#M3362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;OL&gt;&lt;LI&gt;I&amp;nbsp;want to send more than two CAN messages, I encountered an error: MSCAN0 error Module of MSCAN0 Transmit block 'Tem_Test/CAN_Sub/CAN_Transmit' is shared with Module of another MSCAN0 Transmit block;&lt;/LI&gt;&lt;LI&gt;so I follow the tutorial below to fix this bug, But when I modified the file ***MSCAN0_check.p→ ***.none, I encountered a new error, what should I do? Please help me, thank you.&lt;/LI&gt;&lt;LI&gt;I use matlab 2015a&lt;/LI&gt;&lt;LI&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86903iFF36BA7B61682A6B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;LI&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86906i76E2A81AF088D16A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 07:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Error-with-MBDT-for-9s12zvc/m-p/919329#M3362</guid>
      <dc:creator>xuxingwen0719</dc:creator>
      <dc:date>2019-06-13T07:38:31Z</dc:date>
    </item>
    <item>
      <title>Re: Error with MBDT for 9s12zvc？？？？？</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Error-with-MBDT-for-9s12zvc/m-p/919330#M3363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi community;&lt;/P&gt;&lt;P&gt;The problem has been found to be a solution. as follows:&lt;BR /&gt;1. Follow this step to repair the .c file with the following address: "https://community.nxp.com/thread/450789";&lt;BR /&gt;2, mbd_s12zvc_block_mscan0_check.p file can not be directly modified to .none, you need to use the following attachment to replace;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2019 08:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Error-with-MBDT-for-9s12zvc/m-p/919330#M3363</guid>
      <dc:creator>xuxingwen0719</dc:creator>
      <dc:date>2019-06-14T08:06:56Z</dc:date>
    </item>
  </channel>
</rss>