<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: MPC5744P Flashing</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744P-Flashing/m-p/918342#M3358</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/onuralp"&gt;onuralp&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using our toolbox!&lt;/P&gt;&lt;P&gt;Indeed the DEVKIT uses the OpenSDA as debugger. But for this board it is also used as an USB2Serial.As far as I understand, you want to use the MCU without this OpenSDA on your custom board. You can use any USB2Serial for&amp;nbsp;flashing the mcu by using the same UART pins. Also, you can use the JTAG&amp;amp; S32DS for Power Architecture to program the flash but for this you need to manually flash the .mot file after the Simulink built the generated code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please send me the EVB revision in order to tell which are the UART pins needed to be connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Marius&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Aug 2019 14:52:24 GMT</pubDate>
    <dc:creator>mariuslucianand</dc:creator>
    <dc:date>2019-08-29T14:52:24Z</dc:date>
    <item>
      <title>MPC5744P Flashing</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744P-Flashing/m-p/918341#M3357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm a bit new&amp;nbsp;on embedded systems so, sorry if I'm wrong or misunderstand something. I want to use MPC5744P on my project and i bought &lt;A href="https://www.nxp.com/design/development-boards/automotive-development-platforms/mpc57xx-mcu-platforms/development-board-for-mpc5744p:DEVKIT-MPC5744P"&gt;DEVKIT-MPC5744P&lt;/A&gt;.&amp;nbsp; With development kit I'm able to program the MCU from MATLAB via serial port. I searched a little bit and as i understand, for this communication devkit uses a secondary MCU to flash the MPC5744P. But for my project, I don't want to use a secondaru MCU for flashing. I would like to know if I&amp;nbsp;there is any debugger or something to&amp;nbsp;communicate and flash MCU with MATLAB. Thank you already.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 07:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744P-Flashing/m-p/918341#M3357</guid>
      <dc:creator>onuralp</dc:creator>
      <dc:date>2019-08-29T07:45:41Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P Flashing</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744P-Flashing/m-p/918342#M3358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/onuralp"&gt;onuralp&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using our toolbox!&lt;/P&gt;&lt;P&gt;Indeed the DEVKIT uses the OpenSDA as debugger. But for this board it is also used as an USB2Serial.As far as I understand, you want to use the MCU without this OpenSDA on your custom board. You can use any USB2Serial for&amp;nbsp;flashing the mcu by using the same UART pins. Also, you can use the JTAG&amp;amp; S32DS for Power Architecture to program the flash but for this you need to manually flash the .mot file after the Simulink built the generated code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please send me the EVB revision in order to tell which are the UART pins needed to be connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Marius&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 14:52:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5744P-Flashing/m-p/918342#M3358</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2019-08-29T14:52:24Z</dc:date>
    </item>
  </channel>
</rss>