<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Dwarf Section Corupted in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Dwarf-Section-Corupted/m-p/897175#M3147</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using a KV31F120M, MBD Toolbox and a GCC Toolchain. I can build, download and execute models on the device. I setup a connection wih Freemaster over UART as well. Whenever I try to add the .elf in options-&amp;gt;MAPfiles I get the prompt saying: "Dwarf Section corupted". This happens no matter what project I build (Simple, Complex, Examples from the Toolbox). I assume there is something wrong with the settings of the Toolchain?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will gladly provide any Information about my settings.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Apr 2019 10:28:40 GMT</pubDate>
    <dc:creator>pbgemann001</dc:creator>
    <dc:date>2019-04-16T10:28:40Z</dc:date>
    <item>
      <title>Dwarf Section Corupted</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Dwarf-Section-Corupted/m-p/897175#M3147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using a KV31F120M, MBD Toolbox and a GCC Toolchain. I can build, download and execute models on the device. I setup a connection wih Freemaster over UART as well. Whenever I try to add the .elf in options-&amp;gt;MAPfiles I get the prompt saying: "Dwarf Section corupted". This happens no matter what project I build (Simple, Complex, Examples from the Toolbox). I assume there is something wrong with the settings of the Toolchain?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will gladly provide any Information about my settings.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Apr 2019 10:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Dwarf-Section-Corupted/m-p/897175#M3147</guid>
      <dc:creator>pbgemann001</dc:creator>
      <dc:date>2019-04-16T10:28:40Z</dc:date>
    </item>
    <item>
      <title>Re: Dwarf Section Corupted</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Dwarf-Section-Corupted/m-p/897176#M3148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/pbgemann001@ikasle.ehu.eus"&gt;pbgemann001@ikasle.ehu.eus&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This toolbox was not designed from the beginning to support the GCC hence some issues might occurs.&lt;/P&gt;&lt;P&gt;Can you explain your procedure of trying to generate the map files ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it does not works by adding the arguments in the UI, then we can try to pass is directly from the *.tmf file as a direct argument to the linker.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2019 05:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Dwarf-Section-Corupted/m-p/897176#M3148</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2019-04-19T05:29:46Z</dc:date>
    </item>
    <item>
      <title>Re: Dwarf Section Corupted</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Dwarf-Section-Corupted/m-p/897177#M3149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/dumitru-daniel.popa"&gt;dumitru-daniel.popa&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like the solution was way less complex. I reinstalled the latest version of Freemaster and now it works fine. &lt;BR /&gt;Thanks for your response anyway!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Apr 2019 10:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Dwarf-Section-Corupted/m-p/897177#M3149</guid>
      <dc:creator>pbgemann001</dc:creator>
      <dc:date>2019-04-21T10:33:22Z</dc:date>
    </item>
  </channel>
</rss>