<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 How to measure the Phase Voltage?</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-measure-the-Phase-Voltage/m-p/668076#M314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Daniel:&lt;/P&gt;&lt;P&gt;Which pin is used to detect the Phase Voltage &amp;nbsp;in the following figure? HS0,HS1,and HS2?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15345i82874D3F0B3F5625/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Besides，&amp;nbsp;Is the phase voltage described above correspond to Ua,Ub and Uc in the flowing figure? &amp;nbsp;Thank you very much ,my friend.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15128iEC2FA1483A18DFB4/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Aug 2017 11:05:08 GMT</pubDate>
    <dc:creator>jiangfeng</dc:creator>
    <dc:date>2017-08-07T11:05:08Z</dc:date>
    <item>
      <title>How to measure the Phase Voltage?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-measure-the-Phase-Voltage/m-p/668076#M314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Daniel:&lt;/P&gt;&lt;P&gt;Which pin is used to detect the Phase Voltage &amp;nbsp;in the following figure? HS0,HS1,and HS2?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15345i82874D3F0B3F5625/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Besides，&amp;nbsp;Is the phase voltage described above correspond to Ua,Ub and Uc in the flowing figure? &amp;nbsp;Thank you very much ,my friend.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15128iEC2FA1483A18DFB4/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Aug 2017 11:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-measure-the-Phase-Voltage/m-p/668076#M314</guid>
      <dc:creator>jiangfeng</dc:creator>
      <dc:date>2017-08-07T11:05:08Z</dc:date>
    </item>
    <item>
      <title>Re: How to measure the Phase Voltage?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-measure-the-Phase-Voltage/m-p/668077#M315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jiangfeng"&gt;jiangfeng&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;I presume you need it for the BLDC sersorless drive based on phase BackEMF zero crossing. At each commutation phase (is you use the standard 2 out 3 phase commutation technique that maximize the torque) you will need to read the HSxxx that corresponds to the un-powered phase. You will need to implement your own logic algorithm to read and update the phase voltage of each phase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of PMSM&amp;nbsp;it is not very helpful since since by default you know/control the amount of voltage that you apply to the motor. Overall in this case might be helpful to know if a transistor is broken.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And, yes - it corresponds to Ua/Ub/Uc phase voltages.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Aug 2017 07:02:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-measure-the-Phase-Voltage/m-p/668077#M315</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-08-08T07:02:05Z</dc:date>
    </item>
  </channel>
</rss>