<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックFreemaster with KV31: Can not detect Board information</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-with-KV31-Can-not-detect-Board-information/m-p/887472#M3034</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my setup is a KV31F120M and the Motor Control Toolbox on Matlab2019a / Windows. I have successfully compiled and downloaded a simple LED example (attached). Now I want to establish a connection to Freemaster.&lt;/P&gt;&lt;P&gt;I did the following:&lt;/P&gt;&lt;P&gt;- Add the Freemaster Data Recorder Block to the Model&lt;/P&gt;&lt;P&gt;- Freemaster Config -&amp;gt; UART1 / Baudrate: 9600&lt;/P&gt;&lt;P&gt;- Build&lt;/P&gt;&lt;P&gt;- Freemaster -&amp;gt; Options -&amp;gt; COM7 (OpenSDA) / Speed: 9600&lt;/P&gt;&lt;P&gt;- Start Communication leads to the ERROR: "Can not detect board Information! Communication will be paused."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any Ideas on how to solve this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Apr 2019 11:40:36 GMT</pubDate>
    <dc:creator>pbgemann001</dc:creator>
    <dc:date>2019-04-08T11:40:36Z</dc:date>
    <item>
      <title>Freemaster with KV31: Can not detect Board information</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-with-KV31-Can-not-detect-Board-information/m-p/887472#M3034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my setup is a KV31F120M and the Motor Control Toolbox on Matlab2019a / Windows. I have successfully compiled and downloaded a simple LED example (attached). Now I want to establish a connection to Freemaster.&lt;/P&gt;&lt;P&gt;I did the following:&lt;/P&gt;&lt;P&gt;- Add the Freemaster Data Recorder Block to the Model&lt;/P&gt;&lt;P&gt;- Freemaster Config -&amp;gt; UART1 / Baudrate: 9600&lt;/P&gt;&lt;P&gt;- Build&lt;/P&gt;&lt;P&gt;- Freemaster -&amp;gt; Options -&amp;gt; COM7 (OpenSDA) / Speed: 9600&lt;/P&gt;&lt;P&gt;- Start Communication leads to the ERROR: "Can not detect board Information! Communication will be paused."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any Ideas on how to solve this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 11:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-with-KV31-Can-not-detect-Board-information/m-p/887472#M3034</guid>
      <dc:creator>pbgemann001</dc:creator>
      <dc:date>2019-04-08T11:40:36Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster with KV31: Can not detect Board information</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-with-KV31-Can-not-detect-Board-information/m-p/887473#M3035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found the solution: Should be UART0 Pin: PTB16 and PTB17&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 13:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-with-KV31-Can-not-detect-Board-information/m-p/887473#M3035</guid>
      <dc:creator>pbgemann001</dc:creator>
      <dc:date>2019-04-15T13:09:38Z</dc:date>
    </item>
  </channel>
</rss>