<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: System clock frequency configuration for Kinetis KV10 MCU's</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/System-clock-frequency-configuration-for-Kinetis-KV10-MCU-s/m-p/870741#M2901</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/m.benderradji@outlook.fr"&gt;m.benderradji@outlook.fr&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately MBDT does not provide a way to configure the clocks registers or to check other variables related with it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But, if your really need to change some settings in clocks, the code generated calls a function called mcg_kv10v_init which can be found in&amp;nbsp;Kinetis\src\mctbx_kv10z\src\c_library\clc_init.c&lt;/P&gt;&lt;P&gt;For each and every time you generate code this file is copied into the generated code and the main function uses the&amp;nbsp;&lt;SPAN&gt;mcg_kv10v_init&amp;nbsp;to init the clock.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Even if you add here variables to edit them with the FreeMaster I think is useless because the clock it is initialized before your app is started. So the only way it is to&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;modify the&amp;nbsp;mcg_kv10v_init&amp;nbsp;to fit your needs.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Marius&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Feb 2019 15:46:58 GMT</pubDate>
    <dc:creator>mariuslucianand</dc:creator>
    <dc:date>2019-02-19T15:46:58Z</dc:date>
    <item>
      <title>System clock frequency configuration for Kinetis KV10 MCU's</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/System-clock-frequency-configuration-for-Kinetis-KV10-MCU-s/m-p/870740#M2900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default the system clock frequency for kinetis KV10 MCU's is 75 MHz.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72391i72AB2B4F3224F95E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could you please tell me if there is a possibility to configure the system clock frequency (use another value instead of 75) ? configuration with PLL for example ?&lt;/P&gt;&lt;P&gt;In FreeMaster, is it possible to have access to the system clock ? if yes, which variable i need to check?&lt;/P&gt;&lt;P&gt;Thanks in advance for your support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2019 15:13:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/System-clock-frequency-configuration-for-Kinetis-KV10-MCU-s/m-p/870740#M2900</guid>
      <dc:creator>m_benderradji</dc:creator>
      <dc:date>2019-02-18T15:13:27Z</dc:date>
    </item>
    <item>
      <title>Re: System clock frequency configuration for Kinetis KV10 MCU's</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/System-clock-frequency-configuration-for-Kinetis-KV10-MCU-s/m-p/870741#M2901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/m.benderradji@outlook.fr"&gt;m.benderradji@outlook.fr&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately MBDT does not provide a way to configure the clocks registers or to check other variables related with it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But, if your really need to change some settings in clocks, the code generated calls a function called mcg_kv10v_init which can be found in&amp;nbsp;Kinetis\src\mctbx_kv10z\src\c_library\clc_init.c&lt;/P&gt;&lt;P&gt;For each and every time you generate code this file is copied into the generated code and the main function uses the&amp;nbsp;&lt;SPAN&gt;mcg_kv10v_init&amp;nbsp;to init the clock.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Even if you add here variables to edit them with the FreeMaster I think is useless because the clock it is initialized before your app is started. So the only way it is to&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;modify the&amp;nbsp;mcg_kv10v_init&amp;nbsp;to fit your needs.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Marius&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 15:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/System-clock-frequency-configuration-for-Kinetis-KV10-MCU-s/m-p/870741#M2901</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2019-02-19T15:46:58Z</dc:date>
    </item>
  </channel>
</rss>