<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックMBDT with Vehicle Network Toolbox build error - Dual CAN RX</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-with-Vehicle-Network-Toolbox-build-error-Dual-CAN-RX/m-p/834678#M2652</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am&amp;nbsp;building off of the FlexCAN Traffic example in the MBDT to create a model that receives multiple CAN messages.&amp;nbsp; I am using a method very similar to what Razvan just happened to post &lt;A _jive_internal="true" href="https://community.nxp.com/thread/488877"&gt;here&lt;/A&gt;.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I am also trying to use the Simulink Vehicle Network Toolbox to unpack the data in the CAN messages into usable signals using a .dbc file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74891i29C077426DF46108/image-size/large?v=v2&amp;amp;px=999" title="Example.png" alt="Example.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In some scenarios I am getting a build error indicating that stack and heap are overlapping.&amp;nbsp; Some scenarios:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Single CAN message RX with multiple signals being unpacked - builds ok&lt;/LI&gt;&lt;LI&gt;Two CAN message RX with a single signal being unpacked from each message - builds ok&lt;/LI&gt;&lt;LI&gt;Two CAN message RX with one signal being unpacked from one&amp;nbsp;message and multiple signals being unpacked from the other message - build fails with error&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I don't use the Vehicle Network Toolbox and manually unpack the data from the CAN message for multiple messages I don't seem to have a problem, although I haven't tried that extensively yet.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Examples of each of the above scenarios are attached, along with a build log showing the error I get in the third scenario.&amp;nbsp; Can someone offer some insight as to what is causing the stack/heap issue and how to avoid it when using the vehicle network toolbox for CAN message unpacking?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy K.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Nov 2018 17:34:21 GMT</pubDate>
    <dc:creator>andyknitt</dc:creator>
    <dc:date>2018-11-14T17:34:21Z</dc:date>
    <item>
      <title>MBDT with Vehicle Network Toolbox build error - Dual CAN RX</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-with-Vehicle-Network-Toolbox-build-error-Dual-CAN-RX/m-p/834678#M2652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am&amp;nbsp;building off of the FlexCAN Traffic example in the MBDT to create a model that receives multiple CAN messages.&amp;nbsp; I am using a method very similar to what Razvan just happened to post &lt;A _jive_internal="true" href="https://community.nxp.com/thread/488877"&gt;here&lt;/A&gt;.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I am also trying to use the Simulink Vehicle Network Toolbox to unpack the data in the CAN messages into usable signals using a .dbc file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74891i29C077426DF46108/image-size/large?v=v2&amp;amp;px=999" title="Example.png" alt="Example.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In some scenarios I am getting a build error indicating that stack and heap are overlapping.&amp;nbsp; Some scenarios:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Single CAN message RX with multiple signals being unpacked - builds ok&lt;/LI&gt;&lt;LI&gt;Two CAN message RX with a single signal being unpacked from each message - builds ok&lt;/LI&gt;&lt;LI&gt;Two CAN message RX with one signal being unpacked from one&amp;nbsp;message and multiple signals being unpacked from the other message - build fails with error&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I don't use the Vehicle Network Toolbox and manually unpack the data from the CAN message for multiple messages I don't seem to have a problem, although I haven't tried that extensively yet.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Examples of each of the above scenarios are attached, along with a build log showing the error I get in the third scenario.&amp;nbsp; Can someone offer some insight as to what is causing the stack/heap issue and how to avoid it when using the vehicle network toolbox for CAN message unpacking?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy K.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 17:34:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-with-Vehicle-Network-Toolbox-build-error-Dual-CAN-RX/m-p/834678#M2652</guid>
      <dc:creator>andyknitt</dc:creator>
      <dc:date>2018-11-14T17:34:21Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT with Vehicle Network Toolbox build error - Dual CAN RX</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-with-Vehicle-Network-Toolbox-build-error-Dual-CAN-RX/m-p/834679#M2653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/andyknitt"&gt;andyknitt&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what I can see, the problem is that you run out of memory. Let me go into a few details regarding our linker file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the top you can find the heap and stack sizes defined:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;STRONG&gt;HEAP_SIZE&lt;/STRONG&gt; = DEFINED(__heap_size__) ? __heap_size__ : 0x00000400;&lt;BR /&gt;&lt;STRONG&gt;STACK_SIZE&lt;/STRONG&gt; = DEFINED(__stack_size__) ? __stack_size__ : 0x00000400;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After those, you can find the memory areas defined (in&amp;nbsp;&lt;STRONG&gt;bold&lt;/STRONG&gt; what's important to your issue):&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Specify the memory areas */&lt;BR /&gt;MEMORY&lt;BR /&gt;{&lt;BR /&gt; /* Flash */&lt;BR /&gt; m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400&lt;BR /&gt; m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010&lt;BR /&gt; m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0003FBF0&lt;/P&gt;&lt;P&gt;/* SRAM_L */&lt;BR /&gt; m_data (RW) : ORIGIN = 0x1FFFE000, LENGTH = 0x00002000&lt;/P&gt;&lt;P&gt;/* SRAM_U */&lt;BR /&gt; &lt;STRONG&gt;m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00001000&lt;/STRONG&gt;&lt;BR /&gt;}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;If we go further, we can see that &lt;STRONG&gt;m_data_2&lt;/STRONG&gt; is comprised of the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;customSectionBlock&lt;/LI&gt;&lt;LI&gt;bss&lt;/LI&gt;&lt;LI&gt;heap&lt;/LI&gt;&lt;LI&gt;stack&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The first 3 sections are placed one after the other in memory, while the stack is placed staring from the end of m_data_2.&lt;/P&gt;&lt;P&gt;At the end we have the following assert&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ASSERT(__StackLimit &amp;gt;= __HeapLimit, "region m_data_2 overflowed with stack and heap")&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;where we check that stack and heap don't overflow. In your case the bss gets so big that pushes the heap over the stack. To bypass this, you can change the HEAP_SIZE or STACK_SIZE, but that depends on what you are looking for. When you're not using that toolbox, the bss is smaller and heap and stack are not overlapping.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to change the heap/stack sizes, the file you'll want to edit is found here:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;STRONG&gt;{ROOT_DIR}\mbdtbx_s32k14x\src\linker\gcc\S32K142_16_flash.ld&amp;nbsp;&lt;/STRONG&gt; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(or &lt;STRONG&gt;_32_flash.ld&lt;/STRONG&gt; at the end, depending on what SRAM you have on your S32K - you can select the option from the main configuration block - MCU tab - SRAM).&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did some tests and found that your application Dual_CAN_Test_Build_Fails works with the following adjustments:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;HEAP_SIZE = DEFINED(__heap_size__) ? __heap_size__ : 0x00000400;&lt;BR /&gt;STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x000003F0;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;So with just a slightly lower value for STACK SIZE, you can make it work - but when you'll make a more complex model that will put more data in the .bss you'll probably get the same error. I can not really know how it's more beneficial for you to manage the heap/stack/bss sizes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S.: in the &lt;STRONG&gt;&amp;lt;model_name&amp;gt;_rtw&lt;/STRONG&gt; folder generated when building a model, you can find the linker file under the name of &lt;STRONG&gt;S32K14x.ld&lt;/STRONG&gt;, regardless of the selected MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope you find this helpful,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Nov 2018 11:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-with-Vehicle-Network-Toolbox-build-error-Dual-CAN-RX/m-p/834679#M2653</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2018-11-15T11:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT with Vehicle Network Toolbox build error - Dual CAN RX</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-with-Vehicle-Network-Toolbox-build-error-Dual-CAN-RX/m-p/834680#M2654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Razvan.&amp;nbsp; Pardon my ignorance, but is there an output of the build process that would allow me to determine how much bss data my model is using so that I can compare different models to try to find the root cause of the excessive usage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Nov 2018 15:06:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-with-Vehicle-Network-Toolbox-build-error-Dual-CAN-RX/m-p/834680#M2654</guid>
      <dc:creator>andyknitt</dc:creator>
      <dc:date>2018-11-19T15:06:37Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT with Vehicle Network Toolbox build error - Dual CAN RX</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-with-Vehicle-Network-Toolbox-build-error-Dual-CAN-RX/m-p/834681#M2655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/andyknitt"&gt;andyknitt&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the generated .map file ( &amp;lt;model_name&amp;gt;.map ) you can see at what addresses the following tags are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;__BSS_END&lt;/P&gt;&lt;P&gt;__BSS_START&lt;/P&gt;&lt;P&gt;__heap_start__&lt;/P&gt;&lt;P&gt;__heap_end__&lt;/P&gt;&lt;P&gt;__stack_start__&lt;/P&gt;&lt;P&gt;__stack_end__&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;From here you can just subtract&amp;nbsp; *END - *START and get your size of all of these.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was now thinking that maybe it would make sense for your application to move sections from SRAM_U (m_data_2) to SRAM_L (m_data). From what I can see you have ~80% free memory from SRAM_L. Maybe it would be useful for you to put the whole .bss section into SRAM_L (m_data) - this way you'll open up SRAM_U (m_data_2) to just be used by heap and stack. Again, this depends on what your application ends up looking like.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can also use readelf if you have something like cygwin installed or on some UNIX OS.&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;readelf --section-details Dual_CAN_Test_Build_Fails.elf&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;If you run the command above, you'll get all sections' information - address, offset, size, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to get only sections from SRAM you can use grep to match 1fff or 2000, depending on which SRAM you want to view:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;readelf --section-details Dual_CAN_Test_Build_Fails.elf | grep -B1 2000&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Using this you'll get something like this:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ readelf --section-details Dual_CAN_Test_Build_Fails.elf | grep -B1 2000&lt;BR /&gt; [10] .bss&lt;BR /&gt; NOBITS 20000000 018000 000810 00 0 0 8&lt;BR /&gt; [11] .heap&lt;BR /&gt; NOBITS 20000810 018000 000400 00 0 0 1&lt;BR /&gt; [12] .stack&lt;BR /&gt; NOBITS 20000c10 018000 0003f0 00 0 0 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The header of the information is the following:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Type&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Addr&amp;nbsp; &amp;nbsp; &amp;nbsp;Off&amp;nbsp; &amp;nbsp; Size&amp;nbsp; &amp;nbsp;ES&amp;nbsp; &amp;nbsp;Lk Inf Al&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 10:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-with-Vehicle-Network-Toolbox-build-error-Dual-CAN-RX/m-p/834681#M2655</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2018-11-20T10:01:23Z</dc:date>
    </item>
  </channel>
</rss>