<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: SVM Block in Automotive Math and Motor Control Library, No DC supply Voltage Input</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SVM-Block-in-Automotive-Math-and-Motor-Control-Library-No-DC/m-p/834209#M2649</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/abhishek.kumar@chassisbrakes.com"&gt;abhishek.kumar@chassisbrakes.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an AMMCLIB block called &lt;STRONG&gt;GMCLIB_ElimDcBusRip&lt;/STRONG&gt; that can be used in front of the SVM block to compensate for the DC bus level.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/834i1E157CD03BC46E6E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default the SVM will generate the reference voltages that are scaled in between 0-1 or (no voltage - DC bus voltage).&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the output of the SVM is 1&amp;nbsp;then this can be translated as: "apply full DC bus voltage on the motor phase"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the&amp;nbsp;&lt;STRONG&gt;GMCLIB_ElimDcBusRip &lt;/STRONG&gt;you can scale the voltage dynamically based on the ADC&amp;nbsp; readings of bus voltage. In case the voltage goes up/down - like during braking or acceleration regimes then you can easily compensate for that behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You final schematic shall look like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79865i95A046796062A3EE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An example of using this block can be found into:&amp;nbsp;&lt;SPAN style="font-family: 'courier new', courier, monospace;"&gt;...\NXP_MBDToolbox_S32K1xx\code\S32_Examples\common\gmclib&lt;/SPAN&gt; folder&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Dec 2018 06:35:18 GMT</pubDate>
    <dc:creator>Daniel_Popa</dc:creator>
    <dc:date>2018-12-06T06:35:18Z</dc:date>
    <item>
      <title>SVM Block in Automotive Math and Motor Control Library, No DC supply Voltage Input</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SVM-Block-in-Automotive-Math-and-Motor-Control-Library-No-DC/m-p/834208#M2648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been going through the modules for PMSM motor Control :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/469934"&gt;Module 7: Torque Control&lt;/A&gt;&amp;nbsp;. In&amp;nbsp; this i came through a block which generates duty cycle for the PWM (as shown in red rectangle).&lt;/P&gt;&lt;P&gt;I want to feed in DC voltage while generating duty cycles. I can not understand how this block can be used without DC voltage supply.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could not find a parameter to define a constant DC supply voltage nor an input port. Am I missing something here?&lt;/P&gt;&lt;P&gt;Please provide your valuable input.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78718i24358896F4DAC91E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 16:03:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SVM-Block-in-Automotive-Math-and-Motor-Control-Library-No-DC/m-p/834208#M2648</guid>
      <dc:creator>abhishek_kumar1</dc:creator>
      <dc:date>2018-12-04T16:03:15Z</dc:date>
    </item>
    <item>
      <title>Re: SVM Block in Automotive Math and Motor Control Library, No DC supply Voltage Input</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SVM-Block-in-Automotive-Math-and-Motor-Control-Library-No-DC/m-p/834209#M2649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/abhishek.kumar@chassisbrakes.com"&gt;abhishek.kumar@chassisbrakes.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an AMMCLIB block called &lt;STRONG&gt;GMCLIB_ElimDcBusRip&lt;/STRONG&gt; that can be used in front of the SVM block to compensate for the DC bus level.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/834i1E157CD03BC46E6E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default the SVM will generate the reference voltages that are scaled in between 0-1 or (no voltage - DC bus voltage).&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the output of the SVM is 1&amp;nbsp;then this can be translated as: "apply full DC bus voltage on the motor phase"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the&amp;nbsp;&lt;STRONG&gt;GMCLIB_ElimDcBusRip &lt;/STRONG&gt;you can scale the voltage dynamically based on the ADC&amp;nbsp; readings of bus voltage. In case the voltage goes up/down - like during braking or acceleration regimes then you can easily compensate for that behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You final schematic shall look like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79865i95A046796062A3EE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An example of using this block can be found into:&amp;nbsp;&lt;SPAN style="font-family: 'courier new', courier, monospace;"&gt;...\NXP_MBDToolbox_S32K1xx\code\S32_Examples\common\gmclib&lt;/SPAN&gt; folder&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2018 06:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SVM-Block-in-Automotive-Math-and-Motor-Control-Library-No-DC/m-p/834209#M2649</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2018-12-06T06:35:18Z</dc:date>
    </item>
    <item>
      <title>Re: SVM Block in Automotive Math and Motor Control Library, No DC supply Voltage Input</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SVM-Block-in-Automotive-Math-and-Motor-Control-Library-No-DC/m-p/834210#M2650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/dumitru-daniel.popa"&gt;dumitru-daniel.popa&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MPC544xP Library but I assume the Math Library works for this too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. I could not find help file (in MATLAB Help or on NXP website) on Automotive Math and Control Library set for&amp;nbsp;&lt;SPAN&gt;MPC544xP. Is it possible to provide a documentation for blocks and what do the parameters means in the blocks?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For example what does "fltModIndex" in "GMCLIB_ElimDcBusRip_FLT", is not explained.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. Could you provide the full web link instead of&amp;nbsp; "&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;..\NXP_MBDToolbox_S32K1xx\code\S32_Examples\common\gmclib".&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;Thank&amp;nbsp;you for the help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;Kindest Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;Abhishek&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2018 08:23:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SVM-Block-in-Automotive-Math-and-Motor-Control-Library-No-DC/m-p/834210#M2650</guid>
      <dc:creator>abhishek_kumar1</dc:creator>
      <dc:date>2018-12-06T08:23:14Z</dc:date>
    </item>
    <item>
      <title>Re: SVM Block in Automotive Math and Motor Control Library, No DC supply Voltage Input</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SVM-Block-in-Automotive-Math-and-Motor-Control-Library-No-DC/m-p/834211#M2651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/begsy"&gt;begsy&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keep in mind that MPC574xP is an older toolbox that will update in February 2019 in order to match the S32K toolbox capabilities, including MATLAB help and various blocks look&amp;amp;feel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the existing MPC574xP toolbox the AMMCLIB block is here:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21334iCB7A91FF966ADEF0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The documentation can be found in the &lt;SPAN style="font-family: 'courier new', courier, monospace;"&gt;...\mbdtbx_pnt\MCLIB_pnt\doc\MPC574XPMCLUG.pdf&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI, the User Manual is also attached. Look at chapter 5.118.4 page 576&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2018 08:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/SVM-Block-in-Automotive-Math-and-Motor-Control-Library-No-DC/m-p/834211#M2651</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2018-12-06T08:36:03Z</dc:date>
    </item>
  </channel>
</rss>