<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ld and Lq measurement  in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Ld-and-Lq-measurement/m-p/794522#M2310</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To measure the Ld and Lq you need to measure the L (total inductance) between phase A in serie with Phase B and Phase C&lt;/P&gt;&lt;P&gt;&amp;nbsp;To do that, you need to measure the current flowing thru phase A in 2 different situations:&lt;/P&gt;&lt;P&gt;- d-axis aligned with phase A (this is easy since the rotor tends to align naturally when the A-phase is magnetized)&lt;/P&gt;&lt;P&gt;- q-axis aligned with phase A (this will be harder since you need to lock the rotor mechanically to maintained the alignment)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once you measure the current waveform for the both cases you can obtain the L value using the raising time and known phase resistance&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74705i51C9E420E8F877C3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only then, using the eq 9 and 10 you will be able to compute the Ld/Lq&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Nov 2018 13:25:04 GMT</pubDate>
    <dc:creator>Daniel_Popa</dc:creator>
    <dc:date>2018-11-12T13:25:04Z</dc:date>
    <item>
      <title>Ld and Lq measurement</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Ld-and-Lq-measurement/m-p/794521#M2309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have read the application note of "PMSM Electrical Parameters Measurement".I'm confused about the equation of inductance measurement at equation 9 and 10.&lt;/P&gt;&lt;P&gt;The total inductance for serial-parallel of the stator winding&amp;nbsp; L will be 3/2 L-theta(electrical theta)?is &lt;SPAN&gt;L-theta the phase inductance?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;so when the electrical angle of rotor is at 0 degree, Ld will be (2/3)L = (2/3)*(3/2)L-theta = L-theta and so does Lq at the 90 degree?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2018 16:43:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Ld-and-Lq-measurement/m-p/794521#M2309</guid>
      <dc:creator>tim960622</dc:creator>
      <dc:date>2018-11-01T16:43:36Z</dc:date>
    </item>
    <item>
      <title>Re: Ld and Lq measurement</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Ld-and-Lq-measurement/m-p/794522#M2310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To measure the Ld and Lq you need to measure the L (total inductance) between phase A in serie with Phase B and Phase C&lt;/P&gt;&lt;P&gt;&amp;nbsp;To do that, you need to measure the current flowing thru phase A in 2 different situations:&lt;/P&gt;&lt;P&gt;- d-axis aligned with phase A (this is easy since the rotor tends to align naturally when the A-phase is magnetized)&lt;/P&gt;&lt;P&gt;- q-axis aligned with phase A (this will be harder since you need to lock the rotor mechanically to maintained the alignment)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once you measure the current waveform for the both cases you can obtain the L value using the raising time and known phase resistance&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74705i51C9E420E8F877C3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only then, using the eq 9 and 10 you will be able to compute the Ld/Lq&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2018 13:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Ld-and-Lq-measurement/m-p/794522#M2310</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2018-11-12T13:25:04Z</dc:date>
    </item>
  </channel>
</rss>