<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: Problem to connect to DEVKIT-MPC5744P with FreeMaster</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-to-connect-to-DEVKIT-MPC5744P-with-FreeMaster/m-p/786008#M2253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My tools: &amp;nbsp;Matlab is 2016a;@ NXP MBDT is 2.0; S32 Design Studio is 2017 R1 with updates&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Build and Download are ok, not able to connect to FreeMaster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tried the Hotfix3 in &lt;A _jive_internal="true" href="https://community.nxp.com/thread/451804"&gt;https://community.nxp.com/thread/451804&lt;/A&gt;. No luck on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tried the solution of &lt;A _jive_internal="true" href="https://community.nxp.com/thread/454868"&gt;https://community.nxp.com/thread/454868&lt;/A&gt;.&amp;nbsp;The FreeMaster&amp;nbsp;works&amp;nbsp;by using RAppID.exe to flash the bin file ADC1.mot under Daniel's comment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please Help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;JD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Jul 2018 00:22:38 GMT</pubDate>
    <dc:creator>jimduanva</dc:creator>
    <dc:date>2018-07-09T00:22:38Z</dc:date>
    <item>
      <title>Problem to connect to DEVKIT-MPC5744P with FreeMaster</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-to-connect-to-DEVKIT-MPC5744P-with-FreeMaster/m-p/786007#M2252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Dimitri,&lt;/P&gt;&lt;P&gt;thank you for this very interesting tutorial. I succeed in installing Model Based Design Toolbox and programming MPC5744P development kit with Simulink. However, I have a problem with Freemaster 2.0 when I try to connect to DEVKIT-MPC5744P.&lt;/P&gt;&lt;P&gt;The message below arises:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65024i464F38F5119F9038/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Even if I load no source file and I try only to connect to the board, when I click to Start/stop communications, this error message arises.&lt;/P&gt;&lt;P&gt;Could you help me to solve this problem ?&lt;/P&gt;&lt;P&gt;Alexandre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jul 2018 14:25:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-to-connect-to-DEVKIT-MPC5744P-with-FreeMaster/m-p/786007#M2252</guid>
      <dc:creator>alexandreboyer</dc:creator>
      <dc:date>2018-07-06T14:25:28Z</dc:date>
    </item>
    <item>
      <title>Re: Problem to connect to DEVKIT-MPC5744P with FreeMaster</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-to-connect-to-DEVKIT-MPC5744P-with-FreeMaster/m-p/786008#M2253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My tools: &amp;nbsp;Matlab is 2016a;@ NXP MBDT is 2.0; S32 Design Studio is 2017 R1 with updates&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Build and Download are ok, not able to connect to FreeMaster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tried the Hotfix3 in &lt;A _jive_internal="true" href="https://community.nxp.com/thread/451804"&gt;https://community.nxp.com/thread/451804&lt;/A&gt;. No luck on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tried the solution of &lt;A _jive_internal="true" href="https://community.nxp.com/thread/454868"&gt;https://community.nxp.com/thread/454868&lt;/A&gt;.&amp;nbsp;The FreeMaster&amp;nbsp;works&amp;nbsp;by using RAppID.exe to flash the bin file ADC1.mot under Daniel's comment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please Help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;JD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2018 00:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-to-connect-to-DEVKIT-MPC5744P-with-FreeMaster/m-p/786008#M2253</guid>
      <dc:creator>jimduanva</dc:creator>
      <dc:date>2018-07-09T00:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: Problem to connect to DEVKIT-MPC5744P with FreeMaster</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-to-connect-to-DEVKIT-MPC5744P-with-FreeMaster/m-p/786009#M2254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had brought the solutions suggested in the different Hotfixes. Everything works after a simple restart of my computer. So, now everythink works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2018 11:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Problem-to-connect-to-DEVKIT-MPC5744P-with-FreeMaster/m-p/786009#M2254</guid>
      <dc:creator>alexandreboyer</dc:creator>
      <dc:date>2018-07-09T11:31:00Z</dc:date>
    </item>
  </channel>
</rss>