<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: Model Based Design Toolbox License Missing</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773341#M2076</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to install matlab, s32ds, mbdt for mpc5744p today,&amp;nbsp; the license error didn't show up,&amp;nbsp; but something else came up ,i am not sure what that means.this is the code generation diagnosic.&lt;/P&gt;&lt;P&gt;"&lt;SPAN&gt;系统找不到指定的路径&amp;nbsp;(The system can not find the specified path.)&lt;/SPAN&gt;"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;### Generating code into build folder: D:\matlab_vcu\adc_ctu_dma_model_mbd_rtw&lt;BR /&gt;### Invoking Target Language Compiler on adc_ctu_dma_model.rtw&lt;BR /&gt;### Using System Target File: D:\Program Files\MBDToolbox\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\mbd_pnt.tlc&lt;BR /&gt;### Loading TLC function libraries&lt;BR /&gt;### Initial pass through model to cache user defined code&lt;BR /&gt;### Caching model source code&lt;BR /&gt;### Writing source file adc_ctu_dma_model.c&lt;BR /&gt;### Writing header file adc_ctu_dma_model_private.h&lt;BR /&gt;### Writing header file adc_ctu_dma_model.h&lt;BR /&gt;### Writing header file adc_ctu_dma_model_types.h&lt;BR /&gt;### Writing header file rtwtypes.h&lt;BR /&gt;.&lt;BR /&gt;### Writing source file mbd_main.c&lt;BR /&gt;### Writing source file intc_sw_vectable.c&lt;BR /&gt;### Writing source file intc_init.c&lt;BR /&gt;### Writing header file bam_defines.h&lt;BR /&gt;### Writing header file target.h&lt;BR /&gt;### TLC code generation complete.&lt;BR /&gt;### Creating project marker file: rtw_proj.tmw&lt;BR /&gt;.### Evaluating PostCodeGenCommand specified in the model&lt;BR /&gt;.&lt;BR /&gt;### Processing Template Makefile: D:\Program Files\MBDToolbox\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\mbd_pnt.tmf&lt;BR /&gt;### Creating adc_ctu_dma_model.mk from D:\Program Files\MBDToolbox\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\mbd_pnt.tmf&lt;BR /&gt;### Building adc_ctu_dma_model: .\adc_ctu_dma_model.bat&lt;BR /&gt; &lt;BR /&gt;D:\matlab_vcu\adc_ctu_dma_model_mbd_rtw&amp;gt;set MATLAB=D:\Program Files\Matlab2016a &lt;BR /&gt; &lt;BR /&gt;D:\matlab_vcu\adc_ctu_dma_model_mbd_rtw&amp;gt;"D:\Program Files\Matlab2016a\bin\win64\gmake" -f adc_ctu_dma_model.mk COPY_MDLREF_INCLUDES=0 GENERATE_ERT_S_FUNCTION=0 INCLUDE_MDL_TERMINATE_FCN=1 COMBINE_OUTPUT_UPDATE_FCNS=1 MULTI_INSTANCE_CODE=0 INTEGER_CODE=0 S32DS_TARGET_DEFAULT_LCF=1 S32DS_TARGET_USER_LCF="MPC5744P_RAM.ld" GHS_TARGET_DEFAULT_LCF=1 GHS_TARGET_USER_LCF="MPC5744P_RAM.ld" DIAB_TARGET_DEFAULT_LCF=1 DIAB_TARGET_USER_LCF="MPC5744P_RAM.lin" ISPROTECTINGMODEL=NOTPROTECTING &lt;BR /&gt;Cleaning... &lt;BR /&gt;RELATIVE_PATH_TO_ANCHOR is .. &lt;BR /&gt;==== Removing object files from build directory ==== &lt;BR /&gt;Copying necessary files to build directory... &lt;BR /&gt;Compiler details : "D:\Program Files\S32DS_Power_v2017R1/Cross_Tools/powerpc-eabivle-4_9/bin/powerpc-eabivle-gcc" -DMPC574xP -mcpu=e200z4 -DSTART_FROM_FLASH --sysroot="D:\Program Files\S32DS_Power_v2017R1/S32DS/e200_ewl2" -g3 -mbig -mvle -O3 -mregnames -mlsp -specs=ewl_c9x.specs -mhard-float -Wall -c -std=c99 -fdata-sections -ffunction-sections -fsigned-char -fmessage-length=0 -nostdinc -I. -I.. -I"D:\Program Files\Matlab2016a\simulink\include" -I"D:\Program Files\Matlab2016a\extern\include" -I"D:\Program Files\Matlab2016a\rtw\c\src" -I"D:\Program Files\Matlab2016a\rtw\c\libsrc" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\common" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\tcpip" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\serial" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\custom" -I"D:\Program Files\S32DS_Power_v2017R1/S32DS/e200_ewl2/EWL_C/include" -I"D:\Program Files\S32DS_Power_v2017R1/S32DS/e200_ewl2/EWL_C/include/pa" -ID:\PROGRA~1\MATLAB~1\simulink\include\sf_runtime -ID:\matlab_vcu\adc_ctu_dma_model_mbd_rtw -ID:\matlab_vcu -DUSE_RTMODEL -DMODEL=adc_ctu_dma_model -DREAL_T=float -DRT -DNUMST=1 -DTID01EQ=0 -DNCSTATES=0 -DMT=0 -DHAVESTDIO &lt;BR /&gt;Assembler details : "D:\Program Files\S32DS_Power_v2017R1/Cross_Tools/powerpc-eabivle-4_9/bin/powerpc-eabivle-as" -g3 -mbig -mvle -mregnames &lt;BR /&gt;Building assembly file crt0.o... &lt;BR /&gt;系统找不到指定的路径。 &lt;BR /&gt;gmake: *** [crt0.o] Error 1&lt;BR /&gt;### Build procedure for model: 'adc_ctu_dma_model' aborted due to an error.&lt;BR /&gt;Build process completed successfully&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Jul 2018 13:09:10 GMT</pubDate>
    <dc:creator>jackjack</dc:creator>
    <dc:date>2018-07-16T13:09:10Z</dc:date>
    <item>
      <title>Model Based Design Toolbox License Missing</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773337#M2072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17527iCA39D85C1877AC5A/image-size/large?v=v2&amp;amp;px=999" title="2018-04-06_210721.png" alt="2018-04-06_210721.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;the hostID is right. I allready get the license, why would that error keeps coming up?&lt;/P&gt;&lt;P&gt;MPC5744P+matlab2016a+s32ds2017&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2018 13:11:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773337#M2072</guid>
      <dc:creator>jackjack</dc:creator>
      <dc:date>2018-04-06T13:11:39Z</dc:date>
    </item>
    <item>
      <title>Re: Model Based Design Toolbox License Missing</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773338#M2073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jackjack"&gt;jackjack&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;Thank you for installing our toolbox.&lt;/P&gt;&lt;P&gt;If you added the license file after you ran the mbd_pnt_path.m script, please set the Matlab path to default and rerun the script (in order to include the license in path).&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can also try to change the extension from .lic to .dat.&lt;/P&gt;&lt;P&gt;Also, please follow this tutorial&amp;nbsp;&lt;A href="https://community.nxp.com/videos/7692"&gt; Video Link : 7692&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Marius&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 06:41:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773338#M2073</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2018-04-11T06:41:05Z</dc:date>
    </item>
    <item>
      <title>Re: Model Based Design Toolbox License Missing</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773339#M2074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i already tried this, but it doesn't work. maybe it has something to do with my driver.&amp;nbsp; i have a 128G SSD(driver C) + 500G HDD(driver D E F). matlab&amp;nbsp; and mbdt are both installed in driver D.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2018 15:15:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773339#M2074</guid>
      <dc:creator>jackjack</dc:creator>
      <dc:date>2018-04-30T15:15:31Z</dc:date>
    </item>
    <item>
      <title>Re: Model Based Design Toolbox License Missing</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773340#M2075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jack,&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the disk serial number of the partition used for MBDT installation (in fact how many numbers does it contains)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2018 16:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773340#M2075</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2018-05-02T16:49:40Z</dc:date>
    </item>
    <item>
      <title>Re: Model Based Design Toolbox License Missing</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773341#M2076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to install matlab, s32ds, mbdt for mpc5744p today,&amp;nbsp; the license error didn't show up,&amp;nbsp; but something else came up ,i am not sure what that means.this is the code generation diagnosic.&lt;/P&gt;&lt;P&gt;"&lt;SPAN&gt;系统找不到指定的路径&amp;nbsp;(The system can not find the specified path.)&lt;/SPAN&gt;"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;### Generating code into build folder: D:\matlab_vcu\adc_ctu_dma_model_mbd_rtw&lt;BR /&gt;### Invoking Target Language Compiler on adc_ctu_dma_model.rtw&lt;BR /&gt;### Using System Target File: D:\Program Files\MBDToolbox\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\mbd_pnt.tlc&lt;BR /&gt;### Loading TLC function libraries&lt;BR /&gt;### Initial pass through model to cache user defined code&lt;BR /&gt;### Caching model source code&lt;BR /&gt;### Writing source file adc_ctu_dma_model.c&lt;BR /&gt;### Writing header file adc_ctu_dma_model_private.h&lt;BR /&gt;### Writing header file adc_ctu_dma_model.h&lt;BR /&gt;### Writing header file adc_ctu_dma_model_types.h&lt;BR /&gt;### Writing header file rtwtypes.h&lt;BR /&gt;.&lt;BR /&gt;### Writing source file mbd_main.c&lt;BR /&gt;### Writing source file intc_sw_vectable.c&lt;BR /&gt;### Writing source file intc_init.c&lt;BR /&gt;### Writing header file bam_defines.h&lt;BR /&gt;### Writing header file target.h&lt;BR /&gt;### TLC code generation complete.&lt;BR /&gt;### Creating project marker file: rtw_proj.tmw&lt;BR /&gt;.### Evaluating PostCodeGenCommand specified in the model&lt;BR /&gt;.&lt;BR /&gt;### Processing Template Makefile: D:\Program Files\MBDToolbox\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\mbd_pnt.tmf&lt;BR /&gt;### Creating adc_ctu_dma_model.mk from D:\Program Files\MBDToolbox\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\mbd_pnt.tmf&lt;BR /&gt;### Building adc_ctu_dma_model: .\adc_ctu_dma_model.bat&lt;BR /&gt; &lt;BR /&gt;D:\matlab_vcu\adc_ctu_dma_model_mbd_rtw&amp;gt;set MATLAB=D:\Program Files\Matlab2016a &lt;BR /&gt; &lt;BR /&gt;D:\matlab_vcu\adc_ctu_dma_model_mbd_rtw&amp;gt;"D:\Program Files\Matlab2016a\bin\win64\gmake" -f adc_ctu_dma_model.mk COPY_MDLREF_INCLUDES=0 GENERATE_ERT_S_FUNCTION=0 INCLUDE_MDL_TERMINATE_FCN=1 COMBINE_OUTPUT_UPDATE_FCNS=1 MULTI_INSTANCE_CODE=0 INTEGER_CODE=0 S32DS_TARGET_DEFAULT_LCF=1 S32DS_TARGET_USER_LCF="MPC5744P_RAM.ld" GHS_TARGET_DEFAULT_LCF=1 GHS_TARGET_USER_LCF="MPC5744P_RAM.ld" DIAB_TARGET_DEFAULT_LCF=1 DIAB_TARGET_USER_LCF="MPC5744P_RAM.lin" ISPROTECTINGMODEL=NOTPROTECTING &lt;BR /&gt;Cleaning... &lt;BR /&gt;RELATIVE_PATH_TO_ANCHOR is .. &lt;BR /&gt;==== Removing object files from build directory ==== &lt;BR /&gt;Copying necessary files to build directory... &lt;BR /&gt;Compiler details : "D:\Program Files\S32DS_Power_v2017R1/Cross_Tools/powerpc-eabivle-4_9/bin/powerpc-eabivle-gcc" -DMPC574xP -mcpu=e200z4 -DSTART_FROM_FLASH --sysroot="D:\Program Files\S32DS_Power_v2017R1/S32DS/e200_ewl2" -g3 -mbig -mvle -O3 -mregnames -mlsp -specs=ewl_c9x.specs -mhard-float -Wall -c -std=c99 -fdata-sections -ffunction-sections -fsigned-char -fmessage-length=0 -nostdinc -I. -I.. -I"D:\Program Files\Matlab2016a\simulink\include" -I"D:\Program Files\Matlab2016a\extern\include" -I"D:\Program Files\Matlab2016a\rtw\c\src" -I"D:\Program Files\Matlab2016a\rtw\c\libsrc" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\common" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\tcpip" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\serial" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\custom" -I"D:\Program Files\S32DS_Power_v2017R1/S32DS/e200_ewl2/EWL_C/include" -I"D:\Program Files\S32DS_Power_v2017R1/S32DS/e200_ewl2/EWL_C/include/pa" -ID:\PROGRA~1\MATLAB~1\simulink\include\sf_runtime -ID:\matlab_vcu\adc_ctu_dma_model_mbd_rtw -ID:\matlab_vcu -DUSE_RTMODEL -DMODEL=adc_ctu_dma_model -DREAL_T=float -DRT -DNUMST=1 -DTID01EQ=0 -DNCSTATES=0 -DMT=0 -DHAVESTDIO &lt;BR /&gt;Assembler details : "D:\Program Files\S32DS_Power_v2017R1/Cross_Tools/powerpc-eabivle-4_9/bin/powerpc-eabivle-as" -g3 -mbig -mvle -mregnames &lt;BR /&gt;Building assembly file crt0.o... &lt;BR /&gt;系统找不到指定的路径。 &lt;BR /&gt;gmake: *** [crt0.o] Error 1&lt;BR /&gt;### Build procedure for model: 'adc_ctu_dma_model' aborted due to an error.&lt;BR /&gt;Build process completed successfully&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jul 2018 13:09:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773341#M2076</guid>
      <dc:creator>jackjack</dc:creator>
      <dc:date>2018-07-16T13:09:10Z</dc:date>
    </item>
    <item>
      <title>Re: Model Based Design Toolbox License Missing</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773342#M2077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;already fixed in&amp;nbsp;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/451804#comment-1008960" title="https://community.nxp.com/thread/451804#comment-1008960"&gt;https://community.nxp.com/thread/451804#comment-1008960&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jul 2018 13:40:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-License-Missing/m-p/773342#M2077</guid>
      <dc:creator>jackjack</dc:creator>
      <dc:date>2018-07-16T13:40:17Z</dc:date>
    </item>
  </channel>
</rss>