<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 5643l ccp with canape in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771698#M2054</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp; When I active the ccp mode in the 5643l configuration block,then generator the code.And Getting the a2l file from canape asap2editor.Then use canape to c&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;alibration.But when I send message to the controller,the controller do not response.Then I use PE to debug,I set breakpoint in the 'ccpCommand((uint8_t*)temp);'.When I use canape send message to the controller,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;the program do not goto the code.The program in the annex.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/123262i97A3A2F6BF09786E/image-size/large?v=v2&amp;amp;px=999" title="207902_207902.png" alt="207902_207902.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57239i069D38D10823E259/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jan 2018 05:44:39 GMT</pubDate>
    <dc:creator>hongjinzeng</dc:creator>
    <dc:date>2018-01-09T05:44:39Z</dc:date>
    <item>
      <title>5643l ccp with canape</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771698#M2054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp; When I active the ccp mode in the 5643l configuration block,then generator the code.And Getting the a2l file from canape asap2editor.Then use canape to c&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;alibration.But when I send message to the controller,the controller do not response.Then I use PE to debug,I set breakpoint in the 'ccpCommand((uint8_t*)temp);'.When I use canape send message to the controller,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;the program do not goto the code.The program in the annex.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/123262i97A3A2F6BF09786E/image-size/large?v=v2&amp;amp;px=999" title="207902_207902.png" alt="207902_207902.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57239i069D38D10823E259/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2018 05:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771698#M2054</guid>
      <dc:creator>hongjinzeng</dc:creator>
      <dc:date>2018-01-09T05:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: 5643l ccp with canape</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771699#M2055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/zenghongjin@chegustech.com"&gt;zenghongjin@chegustech.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before enabling the CCP - have you checked if your CAN networks works?&lt;/P&gt;&lt;P&gt;What i meant to say is: if you configure the MPC5643L to broadcast a CAN message (let's say with a a counter value) can you see that message over the CAN ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2018 06:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771699#M2055</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2018-01-09T06:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: 5643l ccp with canape</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771700#M2056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am sure the CAN network working.Because I &lt;SPAN class=""&gt;transmit&lt;/SPAN&gt; a message through busmaster,meanwhile I can see the message in the window.In this case,The CAN network do not display a error message.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58063i63BE676B34BD06BC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2018 07:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771700#M2056</guid>
      <dc:creator>hongjinzeng</dc:creator>
      <dc:date>2018-01-09T07:20:16Z</dc:date>
    </item>
    <item>
      <title>Re: 5643l ccp with canape</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771701#M2057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see, but i was referring to the CAN on the MPC5643L.&lt;/P&gt;&lt;P&gt;Inside the toolbox there is a CAN example. Does it works on your setup. Can you receive the messages sent from MPC5643L into the Busmaster ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2018 07:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771701#M2057</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2018-01-09T07:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: 5643l ccp with canape</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771702#M2058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After I download the can_simple_block.mdl to the controller,then I use busmaster to observe the message.The message I can receive in the window.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57569iAC9D87F477DB4A7D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2018 07:59:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/5643l-ccp-with-canape/m-p/771702#M2058</guid>
      <dc:creator>hongjinzeng</dc:creator>
      <dc:date>2018-01-09T07:59:30Z</dc:date>
    </item>
  </channel>
</rss>