<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FreeMaster and Simulink FOC/BLDC/PMSM Communication in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754228#M1849</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I come back again.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;We now use ML128 MINI BOARD to drive FOC motor. Do you have any resources to makes &amp;nbsp;FOC motor rotate?&lt;/P&gt;&lt;P&gt;Does the mini board of ML128 can drive a single shunt resistor FOC motor?&lt;/P&gt;&lt;P&gt;Which PART in the FOC/BLDC simulink model or generated C code file &amp;nbsp;is the motor parameters we can input or adjust?&lt;/P&gt;&lt;P&gt;Because I need to change the max voltage and max current for my FOC motor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Furthermore, How can I use ML128 internal oscillator but not the external oscillator on the ML128 MINI BOARD.&lt;/P&gt;&lt;P&gt;Do you have the demo code for switching external to internal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here I attached a source code below which choose external oscillator:&lt;/P&gt;&lt;P&gt;/*****************************************************************************&lt;BR /&gt;*&lt;BR /&gt;* Function: void initCPMU(void)&lt;BR /&gt;*&lt;BR /&gt;* Description: Clock, Reset and Power Management Unit configuration&lt;BR /&gt;*&lt;BR /&gt;*****************************************************************************/&lt;BR /&gt;void initCPMU(void)&lt;BR /&gt;{&lt;BR /&gt; // Wait for stable supply after power up&lt;BR /&gt; while (GDUF_GLVLSF)&lt;BR /&gt; {&lt;BR /&gt; GDUF_GLVLSF = 1;&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;CPMUREFDIV_REFDIV = CPMU_REFDIV;&lt;BR /&gt; CPMUREFDIV_REFFRQ = CPMU_REFFRQ;&lt;BR /&gt; CPMUSYNR_SYNDIV = CPMU_SYNDIV;&lt;BR /&gt; CPMUSYNR_VCOFRQ = CPMU_VCOFRQ;&lt;BR /&gt; CPMUPOSTDIV_POSTDIV = CPMU_POSTDIV;&lt;BR /&gt; &lt;BR /&gt; while (CPMUIFLG_LOCK == 0) &lt;BR /&gt; {&lt;BR /&gt; &lt;BR /&gt; }&lt;BR /&gt; &lt;BR /&gt; CPMURFLG = 0x60; //Clear PORF and LVRF&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thkanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Aug 2018 02:19:18 GMT</pubDate>
    <dc:creator>thomsonzhou</dc:creator>
    <dc:date>2018-08-03T02:19:18Z</dc:date>
    <item>
      <title>FreeMaster and Simulink FOC/BLDC/PMSM Communication</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754224#M1845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anybody know how to make freemaster communiate with simulink model?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working at a project, which needs freemaster work with Simulink models together.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 08:18:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754224#M1845</guid>
      <dc:creator>thomsonzhou</dc:creator>
      <dc:date>2018-06-06T08:18:42Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster and Simulink FOC/BLDC/PMSM Communication</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754225#M1846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/thomsonzhou"&gt;thomsonzhou&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure i understood your scenario. What exactly you wish to achieve?&lt;/P&gt;&lt;P&gt;Currently, the Simulink model contain the options to enable the FreeMASTER embedded driver support on the board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once you have generated the code, the FreeMASTER driver is linked with your application if you can connect the FreeMASTER UI with the board via the selected communication channel to read/write data to the target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you want a different scenario?&lt;/P&gt;&lt;P&gt;1: To have the Simulink dumpling simulation results to FreeMASTER instead of standard Simulink Blocks ?&lt;/P&gt;&lt;P&gt;2: To have the Simulink reading data from FreeMASTER during board run-time ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 08:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754225#M1846</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2018-06-06T08:33:33Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster and Simulink FOC/BLDC/PMSM Communication</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754226#M1847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how freemaster send speed request command to evl board? Just click stop sign button? I saw it is a connection command.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Shoud I create my own command to start my motor? if yes, is there any pdf to show how to create cmd for motor start?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW, I want to test&amp;nbsp;with simulink FOC modules with Freemaster connection without the evaluation board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is Ok or not?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 08:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754226#M1847</guid>
      <dc:creator>thomsonzhou</dc:creator>
      <dc:date>2018-06-07T08:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster and Simulink FOC/BLDC/PMSM Communication</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754227#M1848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/thomsonzhou"&gt;thomsonzhou&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FreeMASTER has 2 compoments:&lt;/P&gt;&lt;P&gt;- the User Interface (UI) that sits on the Host PC&lt;/P&gt;&lt;P&gt;- the Embedded Communication Driver that is linked with the embedded application that runs on the MCU&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FreeMASTER UI is designed to establish a connection with the MCU once you click on the "Stop Sign Button"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In regards with your concern:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;BTW, I want to test&amp;nbsp;with simulink FOC modules with Freemaster connection without the evaluation board.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;If it is Ok or not?&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The answer is NO, you can't test the FreeMASTER connection without having an evaluation board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In regards with:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P style="border: 0px;"&gt;how freemaster send speed request command to evl board? Just click stop sign button? I saw it is a connection command.&amp;nbsp;&lt;/P&gt;&lt;P style="border: 0px;"&gt;Shoud I create my own command to start my motor? if yes, is there any pdf to show how to create cmd for motor start?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The FreeMASTER is using HTML/JavaScript to implement functions that takes as inputs the values for the User Interface and write them into the target by modifying the RAM value for the variable assigned in the function. Please refer to chapter 6 in the document attached for examples.&lt;/P&gt;&lt;P&gt;Using the scripting you can implement your own User Interface panel with ActiveX objects to control anything you wish.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2018 07:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754227#M1848</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2018-06-08T07:26:03Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster and Simulink FOC/BLDC/PMSM Communication</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754228#M1849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I come back again.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;We now use ML128 MINI BOARD to drive FOC motor. Do you have any resources to makes &amp;nbsp;FOC motor rotate?&lt;/P&gt;&lt;P&gt;Does the mini board of ML128 can drive a single shunt resistor FOC motor?&lt;/P&gt;&lt;P&gt;Which PART in the FOC/BLDC simulink model or generated C code file &amp;nbsp;is the motor parameters we can input or adjust?&lt;/P&gt;&lt;P&gt;Because I need to change the max voltage and max current for my FOC motor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Furthermore, How can I use ML128 internal oscillator but not the external oscillator on the ML128 MINI BOARD.&lt;/P&gt;&lt;P&gt;Do you have the demo code for switching external to internal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here I attached a source code below which choose external oscillator:&lt;/P&gt;&lt;P&gt;/*****************************************************************************&lt;BR /&gt;*&lt;BR /&gt;* Function: void initCPMU(void)&lt;BR /&gt;*&lt;BR /&gt;* Description: Clock, Reset and Power Management Unit configuration&lt;BR /&gt;*&lt;BR /&gt;*****************************************************************************/&lt;BR /&gt;void initCPMU(void)&lt;BR /&gt;{&lt;BR /&gt; // Wait for stable supply after power up&lt;BR /&gt; while (GDUF_GLVLSF)&lt;BR /&gt; {&lt;BR /&gt; GDUF_GLVLSF = 1;&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;CPMUREFDIV_REFDIV = CPMU_REFDIV;&lt;BR /&gt; CPMUREFDIV_REFFRQ = CPMU_REFFRQ;&lt;BR /&gt; CPMUSYNR_SYNDIV = CPMU_SYNDIV;&lt;BR /&gt; CPMUSYNR_VCOFRQ = CPMU_VCOFRQ;&lt;BR /&gt; CPMUPOSTDIV_POSTDIV = CPMU_POSTDIV;&lt;BR /&gt; &lt;BR /&gt; while (CPMUIFLG_LOCK == 0) &lt;BR /&gt; {&lt;BR /&gt; &lt;BR /&gt; }&lt;BR /&gt; &lt;BR /&gt; CPMURFLG = 0x60; //Clear PORF and LVRF&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thkanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2018 02:19:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754228#M1849</guid>
      <dc:creator>thomsonzhou</dc:creator>
      <dc:date>2018-08-03T02:19:18Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster and Simulink FOC/BLDC/PMSM Communication</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754229#M1850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Daniel,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Would you mind please tell me which evaluation board you use for the foc motor &amp;nbsp;simluink module named&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: rgba(55, 120, 199, 0.0980392); font-size: 13px;"&gt;S12ZVM_FOC_Sensorless.slx.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: rgba(55, 120, 199, 0.0980392); color: #51626f; font-size: small;"&gt;Currently, we have &amp;nbsp;ml128 mini board. according to the NXP official website， ml128 mini board can only run single shunt foc motor &amp;nbsp;or BLDC motor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: rgba(55, 120, 199, 0.0980392); color: #51626f; font-size: small;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: rgba(55, 120, 199, 0.0980392); color: #51626f; font-size: small;"&gt;You said your simulink modules named both FOC and BLDC can run on your evaluation directly. Which board do you use? Or you use different board for&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: rgba(55, 120, 199, 0.0980392); color: #51626f; font-size: small;"&gt;FOC and BLDC motor？&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: rgba(55, 120, 199, 0.0980392); color: #51626f; font-size: small;"&gt;Wait for your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 02:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-and-Simulink-FOC-BLDC-PMSM-Communication/m-p/754229#M1850</guid>
      <dc:creator>thomsonzhou</dc:creator>
      <dc:date>2018-08-16T02:03:22Z</dc:date>
    </item>
  </channel>
</rss>