<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K MBD Toolbox software configuration in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-MBD-Toolbox-software-configuration/m-p/743194#M1743</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/Maciek"&gt;Maciek&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That behavior is due to the fact that you have enabled/checked "Enable Download Code After Build" option, under Code Generation -&amp;gt; PIL and Download Config tab.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39933iAAE1686F4C8BB263/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have that checkbox enabled, the code will be generated, the executable will be built and downloaded to the board, regardless of 'Generate code only' (built-in Simulink parameter) option under the Code Generation tab -- thus the "Coppy CATCH" message (can't find the path to EVB, because you don't have it connected).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you only want to generate the code, either uncheck(disable) the "Enable Download Code After Build" option, either click on the "Generate Code" button from Code Generation tab, on the right of the "Generate code only" checkbox.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40020i1BC2A3D2D12D3527/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.jpg" alt="pastedImage_2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Nov 2017 12:39:54 GMT</pubDate>
    <dc:creator>constantinrazva</dc:creator>
    <dc:date>2017-11-28T12:39:54Z</dc:date>
    <item>
      <title>S32K MBD Toolbox software configuration</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-MBD-Toolbox-software-configuration/m-p/743193#M1742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I've just installed the MBD Toolbox for S32K14x.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Right now I don't have access to S32K114EVB (no stock in Europe) - we are waiting for EVBs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I build the example model 'gpio_s32k14.slx' - it builds ok. Code is generated and then compiler is invoked correctly. But at the end I've got the following:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Generating S-record... &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;"C:\Users\Maciek\Documents\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\code\tools\gcc-arm-none-eabi-4_9/bin/arm-none-eabi-objcopy" -O srec gpio_s32k14.elf gpio_s32k14.mot&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Created S-record: gpio_s32k14.mot &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Building target all&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;*** Created executable: gpio_s32k14.mot&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;### Successful completion of build procedure for model: gpio_s32k14&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;COPY CATCH: Nie można odnaleźć określonego pliku.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;: &amp;gt;&amp;gt; C:\Users\Maciek\Documents\MATLAB\S32K14_Test\gpio_s32k14_mbd_rtw\gpio_s32k14.mot&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Can't download the file to the board.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(after COPY CATCH there is comment that a file can't be found)&lt;/P&gt;&lt;P&gt;Is it normal to end the build with such comment when the EVB board is not connected ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And also: when I check 'Generate Code Only' option in Config Settings - the build ends in similar way (with the same comment 'COPY CATCH etc...'), although only source code is generated and compiler is not invoked (as expected). Is it ok. to end the build like this ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Maciek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Nov 2017 11:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-MBD-Toolbox-software-configuration/m-p/743193#M1742</guid>
      <dc:creator>Maciek</dc:creator>
      <dc:date>2017-11-28T11:47:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K MBD Toolbox software configuration</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-MBD-Toolbox-software-configuration/m-p/743194#M1743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/Maciek"&gt;Maciek&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That behavior is due to the fact that you have enabled/checked "Enable Download Code After Build" option, under Code Generation -&amp;gt; PIL and Download Config tab.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39933iAAE1686F4C8BB263/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have that checkbox enabled, the code will be generated, the executable will be built and downloaded to the board, regardless of 'Generate code only' (built-in Simulink parameter) option under the Code Generation tab -- thus the "Coppy CATCH" message (can't find the path to EVB, because you don't have it connected).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you only want to generate the code, either uncheck(disable) the "Enable Download Code After Build" option, either click on the "Generate Code" button from Code Generation tab, on the right of the "Generate code only" checkbox.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40020i1BC2A3D2D12D3527/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.jpg" alt="pastedImage_2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Razvan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Nov 2017 12:39:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-MBD-Toolbox-software-configuration/m-p/743194#M1743</guid>
      <dc:creator>constantinrazva</dc:creator>
      <dc:date>2017-11-28T12:39:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K MBD Toolbox software configuration</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-MBD-Toolbox-software-configuration/m-p/743195#M1744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for clarification. I didn't notice this option. Now it compiles without any problems/warnings.&lt;/P&gt;&lt;P&gt;Maciek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Nov 2017 19:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K-MBD-Toolbox-software-configuration/m-p/743195#M1744</guid>
      <dc:creator>Maciek</dc:creator>
      <dc:date>2017-11-28T19:26:44Z</dc:date>
    </item>
  </channel>
</rss>